Skip to main content
Saravanan_Mari
Associate III
Apr 27, 2021 12:17 PM UTC
Solved

Flex CAN tx problem

Hello,

I am working on a SPC560P Discovery Board.

I have imported test application 'SPC560Pxx RLACAN Test Application for Discovery' for FlexCAN testing. In this FlexCAN0 is used in loop back mode and it is working.

But after disabling loop back mode,I cant see any data on the CAN_TX pin with scope.

I configured the:

  • b[0] as CAN0TXD output and b[1] as CAN0RXD input in the pinmap wizard
  • Disable loopback mode
  • Enable FlexCAN0 Use External Clock
  • Set: PressDive =3 , PropSeg=2 , PSEG1=4 , PSEG2=7

After i start the application the program gets stuck in the transmit while loop:

  1. while (can_lld_transmit(&CAND1,txmailbox, &txmsg)==CAN_MSG_WAIT){
  2. }�?�?�?�?�?�?

Its seems like that thecan_lld_is_tx_empty function returns FALSE and it breaks the can_lld_transmit function.

Is the mailbox needs any additional configuration or I configured the CAN clock incorrectly?

Thanks for your help and sorry for the the lot questions but I am new to 32bit controller programming.

Regards,

Saravanan Mariyappan

    This topic has been closed for replies.
    zambrano.luigi
    zambrano.luigiBest answer
    ST Employee
    Apr 28, 2021 6:40 AM UTC

    Hi,

    in attachment you can find a CAN project developed for Pictus Discovery in which the CAN transceiver on the board is connect with a CAN analyzer (it is a module based on another SPC5 platform with a CAN transceiver that is able to catch the CAN flow and send it to an host PC via serial port, in order to analyze on the host the CAN flow). Please, check in this project how the CAN pin are configured and how the CAN driver is configure (especially the baudrate). I can guarantee you that this project has been tested on the hardware and we are able to catch on the host exactly the expected CAN flow. You can find more details about the project within the readme file in the zip.

    Regards,

    Luigi

    21 replies

    Saravanan_Mari
    Associate III
    Apr 29, 2021 4:22 AM UTC

    Please verify the picture for the Baud rate of the Both the Boards

    0693W00000AMpncQAD.png

    zambrano.luigi
    ST Employee
    Apr 29, 2021 6:16 AM UTC

    Hi Saravan,

    the baudrate seems on Pictus seems to be correctly configured to 1M. So, the communication between the 2 boards should be correctly executed. Let me suggest also to try to reduce the baudrate on both boards or, if you have available a second Pictus discovery, to try the communication between the 2 Pictus.

    Regards,

    Luigi

    Saravanan_Mari
    Associate III
    Apr 29, 2021 1:00 PM UTC

    Hi sir,

    Just to highlight again, Can u explain me why this code is stucked in the function can_lld_is_tx_empty function returns FALSE and it breaks the can_lld_transmit function. why it happening

    or

    Normally When this function will return (can_lld_is_tx_empty function) FALSE and it breaks the can_lld_transmit function.

    Saravanan_Mari
    Associate III
    Apr 29, 2021 1:03 PM UTC

    Hi sir,

    Just to highlight again, Can u explain me why this code is stucked in the function can_lld_is_tx_empty function returns FALSE and it breaks the can_lld_transmit function. why it happening

    or

    Normally When this function will return (can_lld_is_tx_empty function) FALSE and it breaks the can_lld_transmit function.

    From my understanding

    1. I think the Transmission Mailbox is not empty that why it not transmitting is my understanding is correct

    zambrano.luigi
    ST Employee
    Apr 30, 2021 5:17 AM UTC

    Hi,

    in the project that I shared, the can_lld_transmit is invoked within a while cycle that try to transmit a packed using the mailbox 1. If the packet is not received by the receiver (STM32), the mailbox will not return free and, on the next call of the can_lld_transmit, the function can_lld_is_tx_empy will return FALSE. In other words, if the receiver doesn't receive the CAN packet, the next one cannot be sent on the same mailbox. The possible issues can be 1. the pin and CAN configuration (from the Pictus Discovery side, I have provided you a project that included these configuration, so the issue could be on the STM32 side) 2. the baudrate 3. the endianess (as already specified, the PPC is a big endian architecture).

    Regards,

    Luigi

    Saravanan_Mari
    Associate III
    Apr 30, 2021 7:34 AM UTC

    Hi sir Thanks for the reply,

    1. Our Team verified that STM32 Board is Working with another STM32 controller via CAN we can Communicate
    2. When we connected the SPC and STM32 the Communication is not established
    3. As you mentioned that the sending the data in while(1) whenever the data is received by the receiver then only next data will send Then i have one doubt in receiver side any acknowledgement is send with acknowledgement only sender going to send the next data is this correct?
    4. Can you send you Receiver code with that we can some idea
    5. In our hand we have only one SPC Discovery Board , Then we need to test with STM32 Board only

    zambrano.luigi
    ST Employee
    Apr 30, 2021 8:38 AM UTC

    Hi Saravanan,

    as explained before, the aim of the project for Pictus Discovery that I shared before is to send some CAN packets through the Pictus CAN transceiver to another board (based on another PowerPC device of the same Pictus family with the same CAN low level driver) that receives the CAN packets from Pictus, converts them in serial packets and transfers them via serial to the host. On the host we have a tool that shows the packets received via serial. In this way we can control the CAN packets sent by the Pictus directly on the host. 

    Now, the firmware on the second board that receives the CAN packets from the Pictus Discovery uses the same CAN low level driver used by the Pictus to trasmit the CAN packets. Since the baudrate of the CAN on Pictus Discovery is 1M, the same baudrate is configured also on this second board (please, see the configuration in attachment).

    0693W00000AMyYWQA1.pngMoreover, the code used to receive the CAN packets from the Pictus Discovery is the following:

    void flexcan1000_Fifo_RX(CANDriver *canp, CANRxFrame crfp) {
     
     data_send(crfp);
     (void) canp;
    }
     
    void data_send(CANRxFrame crfp) {
     
     uint8_t buffer[18];
     uint8_t i;
     for (i=0;i<18;i++){
     	buffer[i] = 0x00;
     }
     *((uint16_t *)buffer) = crfp.TIME;
     buffer[2] = crfp.LENGTH;
     buffer[3] = crfp.RTR;
     buffer[4] = crfp.TYPE;
     //buffer += 5;
     *((uint32_t *)&buffer[5]) = crfp.ID;
     *((uint32_t *)&buffer[9]) = crfp.data32[0];
     *((uint32_t *)&buffer[13]) = crfp.data32[1];
     buffer[17] = 0xA4;
     sd_lld_write(&SD1, buffer, 18);
    }
     
    int main(void) {
     
     /* Initialization of all the imported components in the order specified in
     the application wizard. The function is generated automatically.*/
     componentsInit();
     
     /* Enable Interrupts */
     irqIsrEnable();
     
     /* Start Serial Driver */
     sd_lld_start(&SD1, NULL);
     
     /* Start CAN Driver */
     can_lld_start(&CAND1, &can_config_flexcan1000);
     
     
     /* Application main loop.*/
     for (;;) {
     
     }
    }

    where flexcan1000_Fifo_RX is the RX callback of the CAN low level driver used to receive the packets from the Pictus Discovery.

    Finally, the CAN low level driver used on the second board has been a little bit patched to receive all the packets sent by the Pictus. You can find it in attachment.

    Regards,

    Luigi

    Jde A.1
    Visitor II
    Feb 21, 2022 11:53 AM UTC

    Dear Luigi,

    I think we are facing the same issue. Where can I find the zip file you refer?

    Thank you very much,

    José

    zambrano.luigi
    ST Employee
    Feb 21, 2022 12:26 PM UTC

    Hi Jose',

    please, check the attachment.

    Regads,

    Luigi

    Jde A.1
    Visitor II
    Feb 21, 2022 1:58 PM UTC

    Thanks a lot!!

    MAli.6
    Associate
    May 19, 2023 5:38 AM UTC

    Hi @Saravanan_Mari​,

    Did you manage to solve this problem since I am also facing the same problem. Already spent weeks trying to solve the issue but CAN0TXD pin remains high and no data out.

    Regards,

    Mian