Skip to main content
CJadh
Associate
Jan 13, 2021 2:06 PM UTC
Solved

Flash write in SPC58B70E5 not working if hex file is written on Flash

Hi,

In the sample application for SPC584BXXX flash test, the hex file is written on RAM and then executed. I need the hex file to get written on flash and then write some data on other specific sectors of flash. So I modified the linker script by changing the RAM sections by flash at some places but the program doesn't work as expected.

Please help me to get an appropriate solution so that the hex gets written on flash and the FlashWrite Flashinit, FlashErase etc. will work as expected.

Thanks in advance.

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Feb 4, 2021 8:51 AM UTC

    Hello ,

    If you are using SPC5Studio.

    Linker file is automatically generated

    you have to create a linker file user.ld at the root of the projet (Cf attachement user.log for an example RAM Sections changing)

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Feb 4, 2021 8:51 AM UTC

    Hello ,

    If you are using SPC5Studio.

    Linker file is automatically generated

    you have to create a linker file user.ld at the root of the projet (Cf attachement user.log for an example RAM Sections changing)

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.