Skip to main content
bin zhuo
Associate
Mar 25, 2022 8:47 AM UTC
Question

[FCCU] use LONG_FUNC_RESET as a fault reaction. how to read fault information, such as which fault channel lead to this long functional reset, after reset?

we are trying to use LONG_FUNC_RESET as a fault reaction. However, I have a problem: how to read fault information, such as which fault channel lead to this long functional reset, after reset? From the FCCU RF_S/ N2FF_STATUS register?

To analysis this, I took the test:

I used Fault Channel #8 for the test, set to LONG_FUNC_RESET, Reset occurs after running the software. The cause of the failure cannot be observed from the RF_S register. The expected result should be the bit position 1 corresponding to Fault Channel #8 (RF_S0 256), not always the default (RF_S0 128, RF_S2 1048576); For the always the default, I set all faults to NO_RESET, and RF_S reads still as above after every time it is reset.0693W00000LviSvQAJ.pnglook forward for feedback, thanks!

my email: 552963005@qq.com

    This topic has been closed for replies.

    1 reply

    bin zhuo
    bin zhuoAuthor
    Associate
    Mar 25, 2022 8:49 AM UTC

    addtion:the chip is SPC58EC80