Skip to main content
stefanodimascio9
Associate III
Nov 14, 2015 2:56 PM UTC
Question

FCCU configuration

Posted on November 14, 2015 at 15:56

Hello everybody, 

I'm using the SPC56EL70L5.Trying to configure the FCCU, I coded:

&sharpdefine CTRLK_OP1 0x913756AF   

&sharpdefine CTRLK_OP2 0x825A132B     //keys needed for operation

&sharpdefine CTRL_OPR1 1    

&sharpdefine CTRL_OPS3 3   

uint32_t FCCU_CONFIG_STATE(void){

    /* ----------------- CONFIG State --------------------- */

    FCCU.CTRLK.R = CTRLK_OP1; /* Key for the operation OP1 */

    FCCU.CTRL.R = CTRL_OPR1;  /* Set the FCCU into the CONFIG state [OP1] */

    while(FCCU.CTRL.B.OPS != CTRL_OPS3);   /* wait for the completion of the operation */

    return 1;

}

But condition is never verified: FCCU.CTRL.OPS is 0x02 (that means operation is aborted) and MCU hangs in the while.

Where is the mistake?

Thanks in advance for the help.

#leopard #fccu #spc56
    This topic has been closed for replies.

    25 replies

    Erwan YVIN
    ST Technical Moderator
    Feb 9, 2016 4:07 PM UTC
    Posted on February 09, 2016 at 17:07

    Hello Stefano ,

    LINFLEX0 (PCTL) is not enabled by default in SAFE/DRUN mode.

    it is the reason why there is abort.

    you should create a function to go in RUN0 mode just before initializing some IPs.

      Best regards

                   Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    stefanodimascio9
    Associate III
    Feb 9, 2016 5:24 PM UTC
    Posted on February 09, 2016 at 18:24

    I don't understand. The device enters RUN0 with hal_lld_init() in both cases.

    stefanodimascio9
    Associate III
    Feb 10, 2016 10:05 AM UTC
    Posted on February 10, 2016 at 11:05

    The only difference I've found is that in sdStart()

      ME.PCTL[n].R = pctl;

    0x00001B68:   70 18 E3 FD  E_LIS     R0,0xC3FD

    0x00001B6C:   18 06 D1 C0  E_ORI     R6,R0,0xC000

    0x00001B70:   C7 01        SE_LWZ    R0,0x1C(R1)

    0x00001B72:   74 07 06 3F  E_RLWINM  R7,R0,0x0,0x18,0x1F

    0x00001B76:   C6 01        SE_LWZ    R0,0x18(R1)

    0x00001B78:   04 60        SE_ADD    R0,R6

    0x00001B7A:   18 00 80 C0  E_ADDI    R0,R0,0xC0

    0x00001B7E:   01 06        SE_MR     R6,R0

    0x00001B80:   90 76        SE_STB    R7,0x0(R6)

    in the first case sets 0x11 in ME_PCTL48 and then the debugger shows the content of LINFLEX0, while in the second case 0x11 is asserted and the debugger still shows unknown content, as if LINFLEX is not clocked anyway or something. I think I'm not configuring in the right way some other register i need to, but I can't find which ones. 

    Erwan YVIN
    ST Technical Moderator
    Feb 10, 2016 10:28 AM UTC
    Posted on February 10, 2016 at 11:28

    Hello Stefano ,

    i was not clear.

    i have reproduced your issue.. the clock was not initialized in SAFE mode.

    In fact, SPC5-HAL is not designed to work in SAFE Mode after Critical Fault.

    1) Please Remove

    for
    the Pre-Clock Initialization Code
    if
    (ME.GS.B.S_CURRENT_MODE != 2) {
    Post-Clock Initialization Code :
    {

    2) Add this following code in hal_lld.c, main.c (it is just for test)

    (cf attachment)

    it is working in my side..

    you have to force the transition SAFE ==> DRUN ==> RUN0

    Best regards

    Erwan

    ________________

    Attachments :

    hal_lld.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0JC&d=%2Fa%2F0X0000000ba6%2FtfRwcDJRNUSmrPEmtHomRpAembLSXP3K1TGbqqu4V6s&asPdf=false

    main.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Tu&d=%2Fa%2F0X0000000ba7%2FgNPMc0AdllYARMyC0vhNoVOSr3gZv1ps4kH2mIM5Djk&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    stefanodimascio9
    Associate III
    Feb 26, 2016 8:39 AM UTC
    Posted on February 26, 2016 at 09:39

    Yes, now it works perfectly.

    Thank you very much.