Skip to main content
saswatkd
Associate
Apr 23, 2015 3:36 PM UTC
Question

Facing issue with LINFLEX_0: Help needed

Posted on April 23, 2015 at 17:36

Hi,

I am writing a LINFLEX_0 driver for SPC560B60L3. DMA is not used as of now. All interrupts are disabled.

Linflex_0 can be configured in 2 sets of port pins

set 1: LIN0TX in PB[0] and LIN0RX in PB[1]. Alternate function in PB[0] is 3.

set 2: LIN0TX in PB[2] and LIN0RX in PB[3]. Alternate function in PB[0] is 1.

If i use set2 i could see the LIN signals in the lin bus. However if i use set1 i do not see any lin signal. I checked the microcontroller pins using oscilloscope and did not see any signal.

I am writing the functions used as mentioned below.

int main (void)

{

   

    __DI(); // Disable All interrupts

   

    Disable_Watchdog();

    MCU_Mode_Init();

    MCU_PLL_Init();

    /* RUN0 Module Config*/

    ME.ME_RUN_MC[0].B.FXOSCON=1;

    ME.ME_RUN_MC[0].B.FMPLLON=1;

    ME.ME_RUN_MC[0].B.SYSCLK=4;

   

    ME.RUN_PC[0].B.RUN0 = 0x1;

    ME.PCTL[48].R = 0x00;

    ME.PCTL[49].R = 0x00;

    ME.PCTL[68].R = 0x00;

   

   /* DRUN-> RUN0 Transition*/

    MCU_SetRunMode(4);

 

 

#if 0

   /* Non Working PORT COnfiguration */

 SIU.PCR[16].B.PA =  0x3;

 SIU.PCR[17].B.IBE = 0x1;

 SIU.PSMI[62].B.PADSEL = 0x1;

#else

   /* Working PORT COnfiguration */

 SIU.PCR[18].B.PA =  0x1;

 SIU.PCR[19].B.IBE = 0x1;

 SIU.PSMI[62].B.PADSEL = 0x0;

  

#endif

 

   LIN_InitChannel ( );

   LIN_SendHeader( );

    /* Enable global interrupt */

    __EI();

   

 

    while(1);

}

void LIN_InitChannel(  void )

{

 

    LINCR1.B.INIT=1;       /* Put the Device into Initialization mode*/

    LINCR1.B.SLEEP = 0;        /* sleep mode cleared*/

    LINCR1.B.MBL =10;      /* 20 bit synch */

    LINCR1.B.MME=1;        /* enable master mode*/

    LINCR1.B.SFTM = 0; /* disabled self test mode*/

    LINCR1.B.LBKM = 0; /* Enabled loop back mode */

    LINFLEX_Ptr->LINFBRR.B.DIV_F=0x5;       /* Write fractional part first*/

    LINFLEX_Ptr->LINIBRR.B.DIV_M=0xD0;

    LINFLEX_Ptr->LINCR1.B.INIT=0;

}

void LIN_SendHeader(void)

{

    LINFLEX_Ptr->BDRL.B.DATA0=0xF0;

    LINFLEX_Ptr->BDRL.B.DATA1=0xF0;

    LINFLEX_Ptr->BDRL.B.DATA2=0xF0;

    LINFLEX_Ptr->BDRL.B.DATA3=0xF0;

    LINFLEX_Ptr->BDRM.B.DATA4=0xF0;

    LINFLEX_Ptr->BDRM.B.DATA5=0xF0;

    LINFLEX_Ptr->BDRM.B.DATA6=0xF0;

    LINFLEX_Ptr->BDRM.B.DATA7=0xF0;

    LINFLEX_Ptr->BIDR.B.ID=9;   /* ID without Parity*/

    LINFLEX_Ptr->BIDR.B.CCS=1;  /* Checksum  0- enhanced, 1- classic*/

    LINFLEX_Ptr->BIDR.B.DFL=7;  /* Number of data bytes in the response part of the frame*/

    LINFLEX_Ptr->BIDR.B.DIR=1;

    LINFLEX_Ptr->LINCR2.B.HTRQ = 1;         /* Request header transmission */

/* If i check the LINS bit for 7, which should be the ideal case, it hangs up.

 So i an checking for 6. Atleast i could see something in the bus */

    while(LINFLEX_Ptr->LINSR.B.LINS!=0x6);

}

I just tried to give a simple version of the driver here. Main point is it is working in 1 set of port and not working in the other.

Compiler used is : Greenhills 6.1.6

Any help and hints would be highly appreciated.

Regards,

Saswat
    This topic has been closed for replies.

    3 replies

    Erwan YVIN
    ST Technical Moderator
    Apr 24, 2015 8:52 AM UTC
    Posted on April 24, 2015 at 10:52

    Hello Saswat ,

    Do you use a Motherboard and Minimodule or Discovery ?

    Did you try to set the OBE for B[0]

    SIU.PCR[16].B.OBE =  1;

       Best regards

                  Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    saswatkd
    saswatkdAuthor
    Associate
    Apr 27, 2015 10:44 AM UTC
    Posted on April 27, 2015 at 12:44

    Hi, Thank you for the response. I use a motherboard from ST. I have found the root cause. I could see the Lin signals in the micro pin when they are terminated in a LIN transceiver. In case of the motherboard, the LIN transceiver is connected to PCR 18 and 19. So I could see the signals.

    I hardwired PCR 16 and 17 to the LIN transceiver an I could see the signals there as well :).

    - Saswat

    Erwan YVIN
    ST Technical Moderator
    Apr 28, 2015 7:35 AM UTC
    Posted on April 28, 2015 at 09:35

    Good news ;)

    have a nice day ;)

          Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.