Skip to main content
stefanodimascio9
Associate III
Feb 3, 2016 9:26 AM UTC
Question

External clock source

Posted on February 03, 2016 at 10:26

Hello everybody,

I am using the external clock option in a evaluation board for the SPC56EL70L5. Thus, I selected ''Oscillator bypass'' in configuration.xml. Even the example projects don't work with that option, while if I left it unselected the examples work only if i put the external clock (this makes me think that because of my jumper configuration I am already working with the external clock).  

The stack with oscillator bypass is attached.

Thank you very much.

  
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Feb 9, 2016 10:28 AM UTC
    Posted on February 09, 2016 at 11:28

    Hello Stefano ,

    Did you try to unplug Y1 ?

    cf Chapter 3.4

    Y1 is a 40MHz thru-hole crystal. The crystal is plugged in a dedicated socket and it can be replaced without using a soldering station.

       Best Regards

                              Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.