Skip to main content
Marco Perciavalle
Associate III
January 10, 2017
Question

eSCI and Virtual COM Port (PLS) for SPC653M

Posted on January 10, 2017 at 20:40

Hi,

I have some problems with serial communication with my board. Could someone help me, please?

I have an SPC563M board with SPC5-UDESTK (pls) for debugging. Is this device designed for Serial trasmission by virtual COM Port? If it isn't possible, why the drivers installed on my PC allow me loading VCP (enabling COM Port)? Moreover, is there another way to communicate with board using a serial protocol? I've read in 'RM0015 Reference manual for SPC563MXX' that in this board there are two eSCI ports: how could I use these ports for my purposes? I've thought to use USB physical layer for this, is it right?

Thanks a lot for any answers.

Best regards.

Marco.

#udetsk #spc56xx #serial #drivers #spc563m #sci
    This topic has been closed for replies.

    4 replies

    Erwan YVIN
    ST Technical Moderator
    January 11, 2017
    Posted on January 11, 2017 at 10:01

    Hello Marco ,

    Do you use SPC56EL70L5DISP or MotherBoard / Mini-Module ?

    you should use USB-Serial Cable plugged on your DB9 SCI (JP18/JP20 Jumper)

    Enabling VCP is working only for B/D Discovery Board

    There is a nice example in SPC5Studio Application Wizard

    SPC56ELxx OS-Less Test Application for DiscoveryPlus

                 Best regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Marco Perciavalle
    Associate III
    January 14, 2017
    Posted on January 14, 2017 at 12:51

    Hi Erwan, 

    no, I use SPC563M-DISP. However, thanks for the support. The example in 

    SPC5Studio Application Wizard for SERIAL driver works. 

    I've another question to do: I want to create a new program; I import the right libraries, I active Serial in 'SPC563Mxx Low Level Drivers Component RLA' and I select in eSCI0 the 'serial' option; so I generate the application. The program created doesn't work. Why?

    I've noticed that the folder named 'spc563mxx_board_initialization_component_rla' is different to the one of the example: inner files (board.h, in particular) don't declare several component such as PIN_SCI_A_RX and PIN_SCI_A_TX_1. Is this differences to cause this problem?

    Thanks a lot!

    Best regards

    Marco.

    Marco Perciavalle
    Associate III
    January 15, 2017
    Posted on January 15, 2017 at 18:59

    I've declared missed variables and I've copied the ''main.c'' of the example in my new project: when I flash the board with this program, I obtain the error in the pictures. (pictures from pls UDE)

    0690X0000060MpiQAE.jpg

    0690X0000060MpmQAE.jpg

    note: the example works, instead

    Erwan YVIN
    ST Technical Moderator
    January 17, 2017
    Posted on January 17, 2017 at 09:48

    Hello Marco ,

    I think that you forgot to enable the associated LINFLEX.

    Low Level drivers RLA and Board Initialization Components (Pinmap Wizard)

    when you use any IP in RLA or HAL you should enable it by the component

    otherwise , the IP is not clocked and can generate an assert.

    Compare the 2 configurations

    0690X000006063yQAA.png0690X00000605waQAA.png

        Best regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.