Skip to main content
alberto2399
Associate II
May 3, 2016 10:24 AM UTC
Question

Eclipse Marketplace error

    This topic has been closed for replies.

    5 replies

    Erwan YVIN
    ST Technical Moderator
    May 3, 2016 3:12 PM UTC
    Posted on May 03, 2016 at 17:12

    Hello Cal ,

    the marketplace is working well.

    did you use a proxy or a firewall ?

    Often ,the firewall can lock the marketplace.

    you can try to use directly the update site

    Help ==> Install New Software

      Best regards

                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    alberto2399
    Associate II
    May 4, 2016 9:43 AM UTC
    Posted on May 04, 2016 at 11:43

    Thank you Erwan!

    Could you indicate the update site?

    Cel

    Erwan YVIN
    ST Technical Moderator
    May 4, 2016 11:50 AM UTC
    Posted on May 04, 2016 at 13:50

    Hello cel ,

    The update site is 

    http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio/updates4/

    Normally , it is stored in SPC5Studio configuration

      Best regards

                 Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    alberto2399
    Associate II
    May 4, 2016 12:54 PM UTC
    Posted on May 04, 2016 at 14:54

    I was able to download the compiler. I guess that now I should configure the compiler through the ''external tool configuration''. 

    I probably need the location and the arguments of the compiler and maybe other settings. Could you provide me this information?

    Thanks again,

    Cel

    Erwan YVIN
    ST Technical Moderator
    May 13, 2016 9:29 AM UTC
    Posted on May 13, 2016 at 11:29

    Hello Cel ,

    When you are switching into ppc-freevle-eabi-

    the options are automatically set.

    The compiler update is based on a standard gcc distribution with VLE support.

    You can find gcc 4.9.3 documentation here:

    Best regards

    Erwan

    ________________

    Attachments :

    2016-05-13_112726.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qVg1&d=%2Fa%2F0X0000000bnz%2Fru8T2lCRkB4J1rCCXRN6rQJXgQuW8L.9hY9i.XQZwhQ&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.