Skip to main content
Santhamurthy R
Associate III
Apr 17, 2017 12:12 PM UTC
Solved

ECC for Flash and RAM configuration Issues

Posted on April 17, 2017 at 14:12

Hello All,

I am using SPC560B54L5 board along with SPC studio V5.2.1.

   I want to enable ECC for RAM and Flash memory area for checking the memory corruption. I enabled the corresponding bits for 1-bit and 2-bit ECC in ECR register but I am unable to enable the corresponding interrupt callback function. I referred  to the SPC560Bxx_RLA Test application, and '@How to Find the memory(FLASH) corruption issues in SPC MCUs?'.(from community).   But I am unable to call the corresponding interrupt callbacks.

   Kindly guide me in enabling the ECC interrupts for Flash and RAM. Please share the example test application for enabling ECC for flash and RAM memory.

Thanks in Advance,

Regards,

R.Santhamurthy

#spc5 #spc5studio
    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Apr 25, 2017 3:22 PM UTC
    Posted on April 25, 2017 at 17:22

    Hello ,

    we have not some examples applications on ECC.

    we have a change request to integrate ECC test example on the application wizard

    you can go to the ECSM chapter (chapter 36)

    i think that you should use vetcor35,vector36

    0690X00000606hQQAQ.png

    After configuring your ECSM and enable the interrupts,

    you can use 

    ECC Error Generation Register (EEGR)

    The ECC Error Generation Register is a 16-bit control register used to force the generation

    of single- and double-bit data inversions in the memories with ECC, most notably the SRAM.

    This capability is provided for two purposes:

    ? It provides a software-controlled mechanism for ?injecting? errors into the memories

    during data writes to verify the integrity of the ECC logic.

    ? It provides a mechanism to allow testing of the software service routines associated

    with memory error logging.

                 Best regards

                              Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Apr 25, 2017 3:22 PM UTC
    Posted on April 25, 2017 at 17:22

    Hello ,

    we have not some examples applications on ECC.

    we have a change request to integrate ECC test example on the application wizard

    you can go to the ECSM chapter (chapter 36)

    i think that you should use vetcor35,vector36

    0690X00000606hQQAQ.png

    After configuring your ECSM and enable the interrupts,

    you can use 

    ECC Error Generation Register (EEGR)

    The ECC Error Generation Register is a 16-bit control register used to force the generation

    of single- and double-bit data inversions in the memories with ECC, most notably the SRAM.

    This capability is provided for two purposes:

    ? It provides a software-controlled mechanism for ?injecting? errors into the memories

    during data writes to verify the integrity of the ECC logic.

    ? It provides a mechanism to allow testing of the software service routines associated

    with memory error logging.

                 Best regards

                              Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.