Skip to main content
stefanodimascio9
Associate III
Feb 17, 2016 10:46 AM UTC
Question

DPM configuration of SPC56EL70L5

Posted on February 17, 2016 at 11:46

This time it's going to be really tough, so every suggestion is well appreciated.

I'm using SPC5 studio and I'd need to run some code just on a single core to avoid any kind of lockstep intervention. So, I need to configure the device in DPM. 

Flashing the device with a modified pattern in the shadow memory lets me connect it with JTAG in DPM with no problem.

Then, starting from a LSM project, in the linker file i put 96 kB instead of 192 kB to handle with the DPM configuration. Now I'll need to add a different MMU initialization , as stated in http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00168395.pdf , but I don't know where. As it is, the MCU hangs at startup and the main is never entered.

The main question is : is it feasibile, starting from a wizard project, of SPC5 studio for LSM to create a DPM working project?

    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Feb 24, 2016 10:21 AM UTC
    Posted on February 24, 2016 at 11:21

    Hello Stefano ,

    Yes .. it is feasible (Cf SPC5-HAL)

    you should inspire from 

    SPC56ECxx OS-Less Z0 Slave Core Test Application

    SPC56ECxx OS-Less Z4 Master Core Test Application

    and create 2 applications using the patch mode

    SPC56ELxx OS-Less Z4 Slave Core Test Application

    SPC56ELxx OS-Less Z4 Master Core Test Application

    I have created a CR to support DPM in EL60.

          Best regards

                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.