Skip to main content
luemy
Associate
Aug 7, 2014 10:03 AM UTC
Solved

Device specific model ''SPC563M64L7'' not supported!

Posted on August 07, 2014 at 12:03

Hello community,

i try to use the PinMap wizard in SPC5 Studio 3 and i receive the meassage ''Device specific model ''SPC563M64L7'' not supported!'' and it seems that there is no support for any model cause i try it with different cpu's.

I use the SPC56M- Discovery board and i'm wondering also that this board is not available in the SPC5Studio Application Wizard.

Any ideas?

Thanks for your help!

- Marc
    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Sep 5, 2014 1:39 PM UTC
    Posted on September 05, 2014 at 15:39

    Hello Marc ,

    the pinmap SPC563M64L7 is ready and is available by update site.

    You can install it from the web by using the command ''Install new software''

        Best Regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    4 replies

    Erwan YVIN
    ST Technical Moderator
    Aug 7, 2014 11:34 AM UTC
    Posted on August 07, 2014 at 13:34

    Hello Marc ,

    SPC5Studio is supported SPC563M64L7 .

    But, the pinmap wizard for SPC563M64L7 is not ready at the current time.

    it should be available in the following weeks.

    (Please check your update site)

    SPC56M- Discovery board is not available on Application Wizard.

    Anyway, if you want to be compliant with SPC56M- Discovery, you can update the application SPC563Mxx OS-Less test application. (EVB with SPC563Mxx Mini Module)

    with good clock settings and update the io settings.

       Best regards

                    Erwan Yvin

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    luemy
    luemyAuthor
    Associate
    Aug 12, 2014 9:25 AM UTC
    Posted on August 12, 2014 at 11:25

    Thanks a lot for the quick answer!

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Sep 5, 2014 1:39 PM UTC
    Posted on September 05, 2014 at 15:39

    Hello Marc ,

    the pinmap SPC563M64L7 is ready and is available by update site.

    You can install it from the web by using the command ''Install new software''

        Best Regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    xqing.1
    Associate II
    May 25, 2024 1:56 AM UTC

    Error: flash driver 'spc563mxx' not found