Skip to main content
Raghu Rajappa
Visitor II
Sep 4, 2017 12:35 PM UTC
Question

Debugging SPC56EL behaves strangely

Posted on September 04, 2017 at 14:35

I have a simple for loop that should ideally run 20 times, inside which I toggle an LED.

When I debug this code on my SPC56EL controller (on a daughter board which is mounted onto the XP56 motherboard) WITHOUT hardware breakpoints, it toggles only once and exits the main handler (confirmed this behavior). But when I add breakpoints in the loop, it works perfectly. Any logical reasoning for such a behavior?

Summarizing - The code works when I put breakpoints in the loop but executes the loop only once when I do not put any breakpoints in the loop. 

#pls #spc56 #32bits #microcontroller
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Sep 4, 2017 3:11 PM UTC
    Posted on September 04, 2017 at 17:11

    Hello Raghu ,

    It is maybe due to the Compiler optimization.

    Which compiler do you use ?

    for such case , it is better to switch in assembler by Mixed Code

    Do you reproduce the issue in some examples applications in SPC5Studio ?

    SPC56ELxx_RLA SERIAL Test Application for DiscoveryPlus

       Best regards

                 Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.