Skip to main content
Yannek
Associate III
Jul 24, 2020 10:08 AM UTC
Solved

Contradiction in SCP5 studio generated code (clock.h)

Hi,

In code generated by SPC5Studio for SPC582B microcontroller there are some macrodifinitions, which validate setting of the clock.

Particularily the one (components\spc582bxx_clock_component_rla\lib\include\clock.h):

/* Check ratio between SPC5_LIN_CLK and PBRIDGE_CLK.*/
#if (SPC5_LIN_CLK != 0U) && (SPC5_PBRIDGE_CLK < ((1UL * SPC5_LIN_CLK) / 3UL) || SPC5_PBRIDGE_CLK > ((2UL * SPC5_LIN_CLK) / 3UL))
#error "SPC5_LIN_CLK outside acceptable range (1/3 PBRIDGE_CLK...2/3 PBRIDGE_CLK)"
#endif

Due to the #if equation - LIN_CLK must be 2 times bigger than PBRIDGE_CLK.

But due to #error comment - LIN_CLK acceptable value is half of PBRIDGE_CLK (between 1/3 and 2/3 of PBRIDGE_CLK actually).

Which one is correct?

Best,

Yannek

    This topic has been closed for replies.
    Giuseppe DI-GIORE
    ST Employee
    Jan 12, 2021 7:32 PM UTC

    Hello,

    actually the relationship is correct while the comment is wrong.

    Reference Manual says: "The relationship “(2/3)* LIN_CLK > PBRIDGEx_CLK > 1/3*LIN_CLK�? should be maintained"

    Regards,

    Giuseppe

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Aug 18, 2020 9:32 AM UTC

    Yes , the error comment does not match with the if

    i am submitting a ER

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Giuseppe DI-GIORE
    ST Employee
    Jan 12, 2021 7:32 PM UTC

    Hello,

    actually the relationship is correct while the comment is wrong.

    Reference Manual says: "The relationship “(2/3)* LIN_CLK > PBRIDGEx_CLK > 1/3*LIN_CLK�? should be maintained"

    Regards,

    Giuseppe