Skip to main content
Associate III
Jun 12, 2022 4:18 AM UTC
Question

Configuration in spi slave mode

Hello.

I'm working with spc560p and I want to enable it's spi slave mode​. All connections are OK but the slave is not working. My code is:

​

for(;;){

spi_lld_start(...)​;

spi_lld_receive(​...,Rxbuf);

spi_lld_stop(...);

​

if(RXbuf == 0xAA){

pal_togglepad;​

}​

}

​

Is there any problem with this code?

Thanks for your attention.

This topic has been closed for replies.

2 replies

Erwan YVIN
ST Technical Moderator
Jun 17, 2022 8:40 AM UTC

Hello ,

I would recommend to use :

spi_lld_exchange(&SPID1, 512, txbuf, rxbuf);

Could you check your assembler code generated by the compiler ?

Other clue is to put a protocol Analyser to check if SPI Frame is well received.

Best regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
DNewm.1Author
Associate III
Jun 19, 2022 8:33 AM UTC

Hello.

In slave mode, ​I just want to read buffers and no sending. With this command I should send something then receive my buffer!

I checked with logic analyzer and master is OK. But my slave is not working. Is there any other ways to receive just rxbuf, how about receive interrupt?

​Thanks