Skip to main content
simone
Associate II
Jan 22, 2016 3:17 PM UTC
Question

Compability issues with UDE

Posted on January 22, 2016 at 16:17

I'm using the MPC5643L from nxp on the modular+minimodule board. Do you know if it is possible to program it with  http://www.st.com/web/en/catalog/tools/PF258744  using the UDE debugger? I apparently can connect but I can't debug and I don't know if it is possible or not.

Thank you very much.

    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Jan 25, 2016 10:34 AM UTC
    Posted on January 25, 2016 at 11:34

    Hello Simon ,

    I think that it should work ...(same device)

    Maybe you need to create a new workspace with Freescale reference with PLS to take the hand.

    (cf screenshot)

    Could you give your minimodule reference ?

    Could you check if PLS FTDI A/B are available in your Windows (Device Manager) after switch-on the board ?

    Best regards

    Erwan

    ________________

    Attachments :

    2016-01-25_113129.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qVW6&d=%2Fa%2F0X0000000bnx%2FBaYroynXZgMeZ1iv_ZsOQ3QrbLlXHJb3DU_7mmGguM8&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.