Skip to main content
Erwan YVIN
ST Technical Moderator
Aug 7, 2017 2:57 PM UTC
Question

community.st.com

Posted on August 07, 2017 at 16:57

SPC5Studio 5.5.0 is available

Dear All ,

SPC5Studio 5.5.0 is available

*** Highlights ***

Here are the changes coming with SPC5Studio v5.5.0

For Mass Market:

===========

-Sphaero (SPC574S) starter kit

Platform component RLA

Board init component RLA

Basic serial RLA driver

Clock component RLA

IRQ Component RLA

OSAL Component RLA

PinMap Wizard

STM, Serial, PIT and EIRQ demos

- Flash driver for SPC57 family

- GTM foundation level for K2 and Lavaredo

- Chorus 6M Starter Kit:

- Minor bugs fixing.

For Selected Customers:

================

- Chorus 6M (SPC58G) starter kit

Platform component RLA

Board init component RLA

LLD component RLA

Clock component RLA

IRQ Component RLA

OSAL Component RLA

PinMap Wizard

- For Chorus 4M (SPC58EC) and 6M (SPC58G)

Ethernet, CAN and DSPI slave mode

New serial driver

DMA

Flash driver

- Power Consumption wizard

Chorus 6M (SPC58EG) support

- Several bugs and improvements, please refer to 

https://community.st.com/community/automotive-mcus-community/spc5-automotive-mcus/activity

 (SPC5Studio part)

*** Notes ***

- Make sure to read the SPC5Studio Users Guide and Components

Writers Guide in

the help section.

Enjoy SPC5Studio,

The SPC5Studio Team.

#spc58 #spc56 #spc5studio #spc57
    This topic has been closed for replies.

    7 replies

    Shen TianHao
    Visitor II
    Aug 24, 2017 3:21 PM UTC
    Posted on August 24, 2017 at 17:21

    Hello,

    I have a computer can not be networked, can you provide an offline upgrade package for SPC5Studio V5.5, or update the SPC5Studio download link to the latest version (V5.0-> V5.5)?

    I want to use the second CAN in Pictus,so I need at least SPC5Studio V5.3 in my offline computer.

    Regards

    Shen

    Erwan YVIN
    ST Technical Moderator
    Aug 25, 2017 10:02 AM UTC
    Posted on August 25, 2017 at 10:02

    Hello Shen ,

    Could you contact your local Field Application Engineer in China for that ?

    i have not the right to provide you due to the license agreement.

    for your information , i have forwarded your request to them.

        Best regards

                    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Yuri Nagornii
    Visitor II
    Sep 19, 2017 8:31 AM UTC
    Posted on September 19, 2017 at 10:31

    Hi all.

    After updating SPC5Studio to ver 5.5 I have a problem with Pin map configurations. Selection of the port and the pin are both not enabled.  You can see in the pictures the previous version, and 5.5.0690X00000608HdQAI.png0690X00000608HYQAY.png

    What could be the reason?

    Erwan YVIN
    ST Technical Moderator
    Sep 19, 2017 2:22 PM UTC
    Posted on September 19, 2017 at 16:22

    Hello Yuri ,

    You should click on Advanced Mode

    (Cf Screenshot)0690X00000608IRQAY.png

       Best regards

                      Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Yuri Nagornii
    Visitor II
    Sep 20, 2017 7:34 AM UTC
    Posted on September 20, 2017 at 09:34

    Hi, 

    Erwan.

    But there isn't a difference.

    0690X00000608J5QAI.png0690X00000608IqQAI.png
    .kasham Arjun
    Visitor II
    Feb 10, 2018 12:49 PM UTC
    Posted on February 10, 2018 at 13:49

    How to get SPC58EC software package?

    Erwan YVIN
    ST Technical Moderator
    Feb 12, 2018 8:43 AM UTC
    Posted on February 12, 2018 at 09:43

    hello ,

    for SPC58x family ,it is for selected customers 

    could you send an email to

    mailto:credentials@spc5studio.com

     ?

    if the marketing guys are ok , we will send you a login/pass for spc58x support

      Best regards

           

                  Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.