Skip to main content
ivancolla9
Associate III
Jan 28, 2016 2:55 PM UTC
Question

Changing GPDI register values with UDE

Posted on January 28, 2016 at 15:55

Good morning to everyone,

I have a little problem with the universal debugger.

In my testing application on the discovery board, I set the reading of a input register 

SIUL.GPDI48.B.PDI.

Now, reading the manual, I understand that is possible, via debugger, change the value of the registers. 

i tried what the guide tells. In the SFR view, I selected the register and tried to change is value, but with no result. 

The register is not protected. If I try to change the value of register as the STM register for exampple, I succed.

Someone has some idea on why it is the case?

Thank you,

Ivan

#ude-debugger-input-registers
    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Feb 1, 2016 3:22 PM UTC
    Posted on February 01, 2016 at 16:22

    Hello Ivan ,

    GPIO Pad Data Input Registers (GPDI) These registers can be used to read the GPIO pad data with a byte access. you can not write

    /**
    * @brief Reads a logical state from an I/O pad.
    * @note The @ref PAL provides a default software implementation of this
    * functionality, implement this function if can optimize it by using
    * special hardware functionalities or special coding.
    *
    * @param[in] port port identifier
    * @param[in] pad pad number within the port
    * @return The logical state.
    * @retval PAL_LOW low logical state.
    * @retval PAL_HIGH high logical state.
    *
    * @notapi
    */
    #define pal_lld_readpad(port, pad) \
    (SIU.GPDI[((port) * 16) + (pad)].R)

    Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ivancolla9
    Associate III
    Feb 1, 2016 4:27 PM UTC
    Posted on February 01, 2016 at 17:27

    Hello Erwan,

    thank you for the advice.

    Regards,

    Ivan