Skip to main content
Visitor II
May 25, 2024 7:50 AM UTC
Solved

changing dcf records

hi i am new to the controller, i read the manual that dcf records contains the configurations like if device boots up it performs some basic tests and then basis on the application address provided in dcf record, it jumps to application, but that address is empty in my case, i want to program it to my application entry point, please tell me how to do this

This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Jun 26, 2024 8:37 AM UTC

Hello Saka ,

Which device do you use SR5 or SPC5?

I recommend to check in the RM.

chapter 9 for SPC52B Line RM

ErwanYVIN_0-1719406918045.png

Often , we are using TRACE32 (script cmm) to update it

         Best Regards

                            Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Jun 26, 2024 8:37 AM UTC

Hello Saka ,

Which device do you use SR5 or SPC5?

I recommend to check in the RM.

chapter 9 for SPC52B Line RM

ErwanYVIN_0-1719406918045.png

Often , we are using TRACE32 (script cmm) to update it

         Best Regards

                            Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Visitor II
Jun 27, 2024 9:27 AM UTC

For SPC5, the program entry address is not set in the DCF records, but in the boot record, which is located in a normal FLASH sector. The boot record usually is (and should be) part of the ELF file. Check the RM for your device to find the supported boot record addresses and fields.

rweiss_0-1719480369033.png

Regards,
Reinhard