Skip to main content
aurelien23
Associate III
Sep 3, 2014 2:46 PM UTC
Question

Change XOSC speed and settings

Posted on September 03, 2014 at 16:46

Hello,

on SPC56EL60, I'm using an external 16MHz XTAL so I changed the ''XOSC Clock'' value in the configuration (default is 40MHz). I'm getting the error:

''SPC5_FMPLL0_VCO_CLK outside acceptable range (SPC5_FMPLLVCO_MIN...SPC5_FMPLLVCO_MAX)''

To solve this I have to modify SPC5_FMPLL0_IDF_VALUE and SPC5_FMPLL0_NDIV_VALUE value's that are used to calculate SPC5_FMPLL0_VCO_CLK.

These defines are code generated and I can't find them in the application config. Can you please explain how the setup the clock peripheral and keep the overide values unchanged while regenerating code?

Thank you
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Sep 5, 2014 8:33 AM UTC
    Posted on September 05, 2014 at 10:33

    Hello Aurélien ,

    Sorry for my late answer,

    at the current time, it is not possible to configure IDF_VALUE and NDIV  in your SPC56ELxx HAL Drivers Component version by  GUI.

    there is a change request about that to add this extended settings

    and the group is set to FALSE:

    (cf below from plugin.xml)

    org.chibios.spc5.components.hal.platform.spc56elxx

    <property

                               brief=''FMPLL0 Input Divider Value.''

                               default=''1''

                               editable=''true''

                               max=''15''

                               min=''1''

                               name=''IDF Value''

                               required=''true''

                               type=''unsigned''>

    </property>

    <property

                               brief=''FMPLL0 Multiplier Value.''

                               default=''32''

                               editable=''true''

                               max=''96''

                               min=''32''

                               name=''NDIV Value''

                               required=''true''

                               type=''unsigned''>

     </property>

    #define SPC5_FMPLL0_IDF_VALUE               ${conf.instance.initialization_settings.fmpll0_settings.idf_value.value[0]} with your defined value

    #define SPC5_FMPLL0_NDIV_VALUE              ${conf.instance.initialization_settings.fmpll0_settings.ndiv_value.value[0]} with defined value

    in waiting for new HAL Drivers with extended settings, i advice you to update this file plugin.xml in your SPC5Studio.

    KEEP THE ORIGINAL ONE

    or use some tips like #undef / #define in your application.

        Best regards

                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.