Skip to main content
brd_gsm
Associate
May 9, 2014
Question

Cant get CAN to work on SPC56xL Discovery + board

Posted on May 09, 2014 at 14:46

Appart from the fact that there are no specific examples for it, i have tried to do something with spc56ELxx OSLess CAN example from another board, and even though leds blink, there is no CAN data generated.

I would really appreciate if i could get this to work.

And regarding FlexRay, are there any resources available for it?

Thanks!

#can-spc56el70l5-flexray
    This topic has been closed for replies.

    9 replies

    Nickname16641_O
    Visitor II
    May 13, 2014
    Posted on May 13, 2014 at 16:15

    Hi,

    The existing CAN demos use an internal loopback mode, messages are exchanged internally so nothing is visible outside.

    If you need to adapt a demo to another board, proceed as follow:

    - Copy/paste the CAN project in the ''Project Explorer'' and give it a new name (optional).

    - Open configuration.xml..

    - Select the ''drivers'' component, go in the CAN section and open the only configuration you see there, unselect the loopback mode.

    - Select the ''board'' component and load the preset for your board using the ''open'' icon in the configuration view, this will setup IOs for your board. You don't need other settings because the two boards have the same oscillatory frequency.

    - In the board component again you have to setup the CAN pins for CAN, see the Reference Manual and the board schematic.

    Giovanni

    Brugus
    ST Employee
    May 19, 2014
    Posted on May 19, 2014 at 17:48

    Hi,

    The CAN - DB9 part assembled in the board is connected in wrong way. To solve the problem you have to add an adapted as indicated in the attached picture.

    Marco

    ________________

    Attachments :

    CAN_DB9_adapter.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qVyu&d=%2Fa%2F0X0000000bo5%2FcS9AGGl25ngKedno93vv9lRCVFuzKMW_rk5hQbN3gnc&asPdf=false
    brd_gsm
    brd_gsmAuthor
    Associate
    May 22, 2014
    Posted on May 22, 2014 at 10:53

    Thank you very much, i will test it this afternoon and come back with results.

    By the way, what about FlexRay?

    Regards,

    Javier

    Nickname16641_O
    Visitor II
    May 29, 2014
    Posted on May 29, 2014 at 08:52

    Hi,

    FlexRay support is not planned for SPC5Studio at this point. A FlexRay driver is available in the AUTOSAR MCAL package for SPC5 devices.

    Giovanni

    David Staffenberger
    Associate II
    June 1, 2017
    Posted on June 01, 2017 at 11:28

    Hello,

    were there any changes regarding FlexRay? Are there any examples for that?

    David

    Erwan YVIN
    ST Technical Moderator
    June 1, 2017
    Posted on June 01, 2017 at 16:37

    Sorry David ,

    At the current time, it is not planned for SPC5Studio release.

               Best Regards

                   Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    David Staffenberger
    Associate II
    June 16, 2017
    Posted on June 16, 2017 at 09:31

    Hello,

    but as far as I understand it still is possible to make use of flexray right?

    Giovanni mentioned the 

    AUTOSAR MCAL package for SPC5 devices, what is this exactly? Is this the drivers for FlexRay?

    Is this something st offers or from a third party?

    Thanks in advance,

    David

    Erwan YVIN
    ST Technical Moderator
    June 16, 2017
    Posted on June 16, 2017 at 10:24

    Hello David ,

    on Mass Market point of view (RLA & HAL), we have no FlexRay drivers

    About AUTOSAR MCAL on SPC56 L, you can find some information on this following link.

    https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/spc5-embedded-software/stsw-spc56as002.license%3d1497601240928.html

       Best regards

                           Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    David Staffenberger
    Associate II
    June 16, 2017
    Posted on June 16, 2017 at 10:55

    Hello Erwan, 

    does this now mean that the SPC56 L can be used for FlexRay applications or not? Because the link you sent does not show any signs of FlexRay. 

    If it is still possible to use the FlexRay is there any possibility that I can get a sample program?

    Best Regards,

    David.