Skip to main content
MPree.1
Visitor II
Apr 26, 2022 5:50 PM UTC
Solved

Can you help out a random student in need of help with his bachelors degree CAN bus task?

I am doing my bachelors degree and have a task to get two boards communicating using the CAN bus. I just got the boards and they pretty much said "have at it" without any prior knowledge.

By now i know most of the really basic stuff about the CAN bus and SPC5Studio but I don't know where to start and what to read. The boards that I got are aek-mot-3p99081 (with the motor) and spc58ec-disp. I also downloaded all of the necessary stuff for the SPC5Studio such as AutoDevKit, MCTK etc. I underastand that i need two terminating resistors and then connect the boards?

I am supposed to load the programs to the board and test them out seperately and then start testing the communication between them using the CAN bus. How can i do it and where to start? And might there be a really bored expert that can help a student out for some weird reason with a call or explanation.

Thank you for reading :).

This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
May 5, 2022 9:41 AM UTC

Hello Mpree ,

Welcom to the SPC5Studio,

all the autodevkit sw stuffs are in the following update site,

http://autodevkit.spc5studio.com/

installable in SPC5Studio 6.0

Best Regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
May 5, 2022 9:41 AM UTC

Hello Mpree ,

Welcom to the SPC5Studio,

all the autodevkit sw stuffs are in the following update site,

http://autodevkit.spc5studio.com/

installable in SPC5Studio 6.0

Best Regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.