Skip to main content
prashanth.mohan22
Associate III
Sep 25, 2019 6:13 AM UTC
Question

can't communicate with target processor

HI,

I'm having PEMicro USB-ML debugger and try connecting it with SPC560B-DIS board.

But I'm not able to connect with the target. I could able to see both target power and USB power glowing in the USB-ML hardware.

As well, I updated the PROGPPCNEXUS firmware. Still not resolved. Please help me over.

0690X000009jAmQQAU.png0690X000009jAmLQAU.png0690X000009jAmGQAU.jpg

Best Regards,

Prashanth Mohan

    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Sep 25, 2019 9:04 AM UTC

    Hello ,

    Sorry,

    I have not PEMicro USB-ML debugger

    Have you checked the jumper settings of Table 3 chap 2.4 of UM1672 SPC560B-DIS discovery board

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    prashanth.mohan22
    Associate III
    Sep 25, 2019 9:39 AM UTC

    HI @Erwan YVIN​ ,

    Thanks for your advice.

    I checked it, so, what I have to do with J19 & J20 (soldered jumpers) for connecting external debugger?

    if it is working for integrated debugger, no change in that jumper configuration should do fine, but it is not. So need help on this.

    0690X000009jBYKQA2.png

    Regards,

    Prashanth