Skip to main content
NBula.1
Associate III
Dec 29, 2020 3:47 PM UTC
Solved

CAN setup in SPC570S-DISP dev board

Hi,

I am trying to setup CAN communication in the SPC570S-DISP dev board. I started with the example available in the SPC5Studio. In the example, internal loopback is enabled, so I disabled it to allow external transmit. I did not change any other settings, as they looked okay to me. In the timing setup section, according to the values that were already set in the example, it has a bit rate of 500 kbps. However, after uploading the code to dev board, and monitoring from a CAN analyzer, no messages seem to be come and the analyzer shows an error. I would like if someone can help me in this matter. I have attached screenshots of the settings and timing setting.

Thank you.

Nisal

0693W000006H6quQAC.png0693W000006H6mUQAS.pngAccording to the clock settings, the CAN clock is set at 40 MHz,

0693W000006H6slQAC.png

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jan 7, 2021 9:30 AM UTC

    Hello ,

    Which CAN Analyzer do you use ?

    there is a Jumper JP7 on the board have you enable it ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    4 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jan 7, 2021 9:30 AM UTC

    Hello ,

    Which CAN Analyzer do you use ?

    there is a Jumper JP7 on the board have you enable it ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    NBula.1
    NBula.1Author
    Associate III
    Jan 7, 2021 10:45 AM UTC

    Hi Erwan,

    I am using the Mircochip CAN bus analyzer. I have enabled the J7 jumper. Any other things I should check ?

    Nisal

    NBula.1
    NBula.1Author
    Associate III
    Jan 15, 2021 12:03 PM UTC

    Hi Erwan,

    Attached here is an image seen from the oscilloscope of the signals CANH and CANL. Please be kind enough to take a look at it.

    Nisal

    0693W000007BQgwQAG.jpg 

    NBula.1
    NBula.1Author
    Associate III
    Jan 15, 2021 12:06 PM UTC

    Here is capture of the CAN RX and CAN TX signals.

    0693W000007BQiTQAW.jpg