Skip to main content
Visitor II
May 29, 2025 6:10 AM UTC
Question

CAN is setting with BusOFF state

Hello Team,

I am currently utilizing the SPC58EC Microcontroller in an Autosar project where I have set up the CAN MCAL driver for both Tx and Rx operations in interrupt mode. We have noticed that whenever the system bus experiences a sending bus load of around 13%(FD and Normal CAN messages are present), the CAN controller which is supported with FD configuration enters a Bus Off state, and this appears to be an intermittent issue . We have two channels configured: one for FD and the other for standard CAN message transmission, with the sample point set at 80%.

When the same software is executed without 2 to 3 necessary messages, the Bus Off state does not occur. SBC TLE 9271 is used as Can Transceiver

This topic has been closed for replies.

1 reply

Erwan YVIN
ST Technical Moderator
Jun 5, 2025 8:16 AM UTC

Hello ,

The issue has been forwarded to Application Team

                 Best Regards

                                   Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.