Skip to main content
nooshin_1382
Associate III
Aug 8, 2015 12:27 PM UTC
Question

Can I use External interrupt Pins for Wakeup?

Posted on August 08, 2015 at 14:27

Hi

I want to use External IRQ Pins for Wake up , Can Use These interrupts or not ?

ex : EIRQ0

Best Regards

Nazerian Vanima
    This topic has been closed for replies.

    4 replies

    ssk
    Associate III
    Aug 10, 2015 5:00 AM UTC
    Posted on August 10, 2015 at 07:00

    Hello,

    Which power down mode you are using? Based on power down mode used, the exit sources are different. Refer section #8.1.3 of reference manual.

    As for using external interrupt, you need to use wakeup module (corresponding wakeup pin) for exiting the stop and standby power down mode.

    Regards,

    Mike.

    nooshin_1382
    Associate III
    Aug 10, 2015 5:41 AM UTC
    Posted on August 10, 2015 at 07:41

    Hi Mike

    Thanks for your response

    I use the STANDBY mode for going to sleep and use wake up pins for gonig to DRUN mode but my problem is the SPC560B50L5 have 19 Wakeup pins and i need 25 Wakeup pin because of this issue i think about external interrup .

    according to Refrence manual i think the MCU did'nt wakeup with external interrupt 

    Best Regards

    Nazerian Vanima

    ssk
    Associate III
    Aug 10, 2015 5:49 AM UTC
    Posted on August 10, 2015 at 07:49

    Yes, wakeup is not possible with external interrupt pins. Instead you can try some decoding logic using available wakeup pins.

    Best Regards,

    Mike.

    Erwan YVIN
    ST Technical Moderator
    Aug 10, 2015 2:46 PM UTC
    Posted on August 10, 2015 at 16:46

    Hello Vanima ,

    From STANDBY mode, wakeup is not possible by EIRQ.

    you should use WKUP Interrupt.

        Best regards

                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.