Skip to main content
hans536
Associate III
Dec 27, 2022 1:45 AM UTC
Solved

Can i run RTOS Task on Multi-core ??

I use spc58nh board.

​

I was using an RTOS Task On one core.

​

I want to use two core, and divide task into two cores.​

​

is this possible?

for example :

core2 - task 1, task 2 --> core 1 - task 1 , core 2 - task 2

​

This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Feb 23, 2023 4:47 PM UTC

Hello ,

Which RTOS do you use ?

we have a nice example in SPC58xNxx_RLA TripleCore Test Application (without RTOS)

Check the application.ld (linker file)

if you want to reserve memory for a core

Best regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

4 replies

hans536
hans536Author
Associate III
Feb 8, 2023 12:47 AM UTC

I did that.

core2-tas1 , task 2 --> core1 - task 1, core2 - task 2

After implementing it like that, the operation that did not work when only core2 worked when divided into core1 and core2.

I don't know if the memory of spc58nh is used separately by core1 and core2.

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Feb 23, 2023 4:47 PM UTC

Hello ,

Which RTOS do you use ?

we have a nice example in SPC58xNxx_RLA TripleCore Test Application (without RTOS)

Check the application.ld (linker file)

if you want to reserve memory for a core

Best regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
hans536
hans536Author
Associate III
Mar 7, 2023 2:59 AM UTC

I use FreeRTOS.

​

thank you. I will refer to tour comments.

​

Associate II
Oct 1, 2024 1:40 PM UTC

Hello @hans536,

Did you get it to put tasks to running in different cores using RTOS?

Best regards.