Skip to main content
jr_it
Associate II
Dec 18, 2014 10:41 AM UTC
Question

C90LC SSD Flash Driver for SPC564B74 Problem

Posted on December 18, 2014 at 11:41

Hello,

since ST did not respond to any license key request, and it is not possible to contact support I will try it here:

I need a license key for C90LC SSD Flash Driver for Programming SPC564B74

Meanwhile I took the C90LC SSD JDP Flash Driver from a Freescale compatible device MPC564xB (where you don't need a fricking license key for any of their drivers).

Since then I have strange problems executing the FlashInit function through JTAG Nexus Interface. Everything works as expected, until leaving Debug mode for executing the function (BTW: which is not only horribly explained but differently done by the PE Micro Nexus Multilink Programmer).

If I do it the way described in AN4365 (

http://cache.freescale.com/files/32bit/doc/app_note/AN4365.pdf?fasp=1

  ) the FlashInit won't be called and CPU will enter Debug mode instantly. In this case the CPUSCR returns: PC: 0xFFFFC004, IR: 0x7C0103A6, CTL: 0x0.

According to PC it's somewhere in the Boot Assist Module hence I assume something went wrong.

The Steps I have done:

- Setup MMU as described in 4.1

- cleared interrupt vectors

- Init SRAM as described in 4.2

- (5.2.2 Step 1) uploaded ssd_config structure to sram start at 0x40000000:

    _ssd_cfg.c90flRegBase = 0xC3F88000;

    _ssd_cfg.mainArrayBase = 0x00000000;

    _ssd_cfg.mainArraySize = 0;

    _ssd_cfg.pageSize = 0x0008;

    _ssd_cfg.shadowRowBase = 0xFFC000;

    _ssd_cfg.shadowRowSize = 0x4000;

    _ssd_cfg.lowBlockNum = 0;

    _ssd_cfg.highBlockNum = 0;

    _ssd_cfg.midBlockNum = 0;

    _ssd_cfg.BDMEnable = 1;

- uploaded C90LC_JDP_SSD FlashInit VLE c_array driver to 0x40000028

- (5.2.2 Step 2) setup r1 as stack pointer to 0x40001FFF

- (5.2.2 Step 3) setup r3 to point to ssd_config structure: 0x40000000

- (5.2.2 Step 4) setup CPUSCR with CTL: 0x00000002,

                                    IR: 0x1800D000,

                                    PC: 0x40000024,

                                   MSR: 0x00000002

- (5.2.2 Step 5) 2.8 Exit from Debug mode:

    - A) Clear OCR[DMDIS], OCR[DR] bits (by writing back previous read and

               both bits cleared value?).

         Note: OCR[MCLK] is referenced at 2.8 as you should leave the bit set,

               but it's not a valid bit of OCR rather it belongs to OSR and

               hence it's read only

    - B) Write CPUSCR (CTL, IR, PC, MSR) (Is this really necessary, since it's

               already done in 5.2.2 Step 4 ?)

    - C) Write OCMD with bits set GO, EX and RS=CPUSCR

         Note: According to this description I would assume that after this

               command DEBUG mode is left and CPU is running. In e200z4

               Reference Manual there it says:

               ''The processor will leave the debug mode after the TAP

               controller Update-DR state is entered.''

               So I assume something is wrong here and a write to CPUSCR is

               needed after that too. So I tried swapping B, and C.

               (that's what PE Micro Nexus Multilink is doing)

- (5.2.2 Step 6) Poll OnCE Status Register (OSR) for re-entering Debug Mode

- (5.2.2 Step 7) read the return value in r3

As I already said: If I do it that way the return value in r3 points still to the ssd_config structure, so FlashInit didn't execute?

CPUSCR is PC: 0xFFFFC004,

          IR: 0x7C0103A6,

         CTL: 0x0

If I do it the way PE Micro Nexus Multilink does (swapping 5.2.2 Step 5: B and C):

when Polling OnCE Status Register (5.2.2 Step 6) the first time I get 1000100001 (MCLK, HALT is set)

then every following time 0100011000 (ERR, STOP, DEBUG is set) and even Bit 9 which should be always 1 is not set.
    This topic has been closed for replies.

    5 replies

    Erwan YVIN
    ST Technical Moderator
    Jan 5, 2015 4:06 PM UTC
    Posted on January 05, 2015 at 17:06

     Hello ehcsur ,

    Sorry for the late answer,

    There is a nice example on Flash integration in SPC5Studio Appwizard

    SPC560Bxx OS-Less Flash Integration Test Application for B64XX

    the Flash driver component integrates C90LC SSD Flash Driver.

    You can try to create SPC560ECxx OS-Less Flash Integration Test Application with B74xx

    and in the Flash Driver component, there is a nice documentation.

       Best regards

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    jr_it
    jr_itAuthor
    Associate II
    Jan 7, 2015 1:45 PM UTC
    Posted on January 07, 2015 at 14:45

    Hello yvin.erwan.001,

    thank you for your answer.

    Is it possible for you to answer my outstanding questions from my initial post?

    I have checked SPC5Studio and there is no SPC560Bxx OS-Less Flash Integration Test Application.

    only the following are available for B74xx:

    • SPC560BCxx OS-Less Test Application
    • SPC560BCxx OS-Less PWM-ICU Test Application
    • SPC560BCxx OS-Less DSPI Example Application
    • SPC560BCxx OS-Less CAN Test Application
    • SPC560BCxx OS-Less ADC Test Application
    • ChibiOS-RT SPC560BCxx Test Application

    Also for other controllers there is no ''... OS-Less Flash Integration Test Application''

    I even doubt that those example would help in this situation since in those examples the CPU is controlled inside from application (assumption) and not via NEXUS Debug interface.

    Regards

    Erwan YVIN
    ST Technical Moderator
    Jan 7, 2015 2:56 PM UTC
    Posted on January 07, 2015 at 15:56

    Hello Ehcsur ,

    Could you update your SPC5Studio ? (cf screenshot)

    B74 is part of SPC560ECxx family.

    Best regards

    Erwan

    ________________

    Attachments :

    2015-01-07_155357.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0YK&d=%2Fa%2F0X0000000baK%2FPk5n8TEMC_JEv08CJUoOgqj6p0Ey7TVbjctS.FF8QsU&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    oayzw
    Visitor II
    Jan 13, 2015 6:55 AM UTC
    Posted on January 13, 2015 at 07:55

    what's different between mpc5604p and spc560p50l3 ?

    the c90lc ssd flash driver run successfully on mpc5604p but failed on spc560p50.

    Thank you very much.

    jr_it
    jr_itAuthor
    Associate II
    Jan 19, 2015 10:29 AM UTC
    Posted on January 19, 2015 at 11:29

    Hello yvin.erwan.001,

    I've updated SPC5Studio and the SPC560Bxx OS-Less Flash Integration Test Application is available now. But as expected the example controls the driver within application running on MCU. Therefore it won't help. I have to control the flash driver via Nexus Debug interface. But as stated the CPU/DEBUG-Registers do not behave as described in documentation. May you please help there?