Skip to main content
Gustav Andersson
Associate II
Feb 8, 2017 1:18 PM UTC
Question

C++ constructor of static objects not called

Posted on February 08, 2017 at 14:18

Hello,

I am trying to use C++ in the SPC560Bxx mcu using SPC5 Studio and the free gcc vle toolchain (4.9.2).

However, it looks like constructors aren't called as I expected.

In the following example, I expect to end up in the first case of the if statement, but I end up in the else case.

class Foo {
public:
 int val;
 Foo() {
 val = 42;
 }
 void do_something() {
 if (val == 42) {
 printf('I expect to end up here');
 } else {
 printf('But I end up here');
 }
 }
};
static Foo myObject; // this ought to call the Foo's constructor

int main(void) {
 ...
 myObject.do_something();�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
 ...
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

From what I understand this is because the crt0.s doesn'tinitialize the static objects on startup.

Does anyone have a solution to my problem or aworking c++ example they can share?

#spc560b54l5 #c++11 #c++ #gcc
    This topic has been closed for replies.

    2 replies

    Gustav Andersson
    Associate II
    Feb 10, 2017 7:08 AM UTC
    Posted on February 10, 2017 at 08:08

    To answer my own question, I found out that if I left the .ctors section during linking and then called each constructor, my problem seems to be solved.

    I had to add the following in the ld-script:

     /* .ctors are used for c++ constructors */
     .ctors :
     {
     PROVIDE(__ctors_start__ = .);
     KEEP(*(SORT(.ctors.*)))
     KEEP(*(.ctors))
     PROVIDE(__ctors_end__ = .);
     } >flash
    �?�?�?�?�?�?�?�?

    and then using the following __late_init function, which is called before main():

    void __late_init() {
     extern void (*__ctors_start__[])(void) __attribute__((weak));
     extern void (*__ctors_end__[])(void) __attribute__((weak));
     int count = __ctors_end__ - __ctors_start__;
     int i;
     for (i = 0; i < count; i++) {
     __ctors_start__[i]();
     }
    }
    �?�?�?�?�?�?�?�?�?�?

    Note that this only solves the construction of global objects.

    Erwan YVIN
    ST Technical Moderator
    Feb 10, 2017 9:40 AM UTC
    Posted on February 10, 2017 at 09:40

    Hello Gustav ,

    I have tried yesterday to port a C Test Application on C++ Test Application in SPC5Studio

    SPC560Dxx OS-Less Test Application for Discovery

    Compilation is ok but i have a coredump on clock init.

    i had forgotten to update my linker file.

    Anyway, i will reactive a change request to create a C++ Test Application from SPC5Studio.

    I will take some time.

    Do not hesitate to contribute on this subject on

      Best regards

             Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.