Skip to main content
nooshin_1382
Associate III
May 27, 2015 9:46 AM UTC
Question

Bug on Spc560b50L5 on SPCstudio in ADC Use

Posted on May 27, 2015 at 11:46

Hi

I Want to read ADC0 channels in SPC560B50L5 but when i use my code or use Spc Function's the mcu have no action , i use this function and test my function with SPC560B54L5 it is work correctly.

I Send my code if any problem exist on this pleaase help me .

If you can get me sample if ADC have not any bug .

Thanks So Much

Best Regards

Vanima Nazerian
    This topic has been closed for replies.

    3 replies

    Erwan YVIN
    ST Technical Moderator
    May 28, 2015 8:42 AM UTC
    Posted on May 28, 2015 at 10:42 Hello Vanima , After Starting the conversion, your program is going to stop the conversion too quickly There are 2 Choices : (Cf

    http://chibios.sourceforge.net/html/group___a_d_c.html

    ) 1) Use the Linear Buffer , after the EOC Callback .. your can let the driver stopping the conversion 2) Use Circular Buffer , you need to stop the conversion.. but let the time of MCU

    /* Starts an ADC continuous conversion.*/
    adcStartConversion(&ADCD1, &adc0_group_cfg0,samples, ADC0_GROUP_CFG0_BUF_DEPTH);
    //adcStart(&ADCD1, NULL);
    init();
    /* Application main loop.*/
    while
    (1)
    {
    /* Let some time to stop the conversion */
    osalThreadSleepMilliseconds(500);
    adcStopConversion(&ADCD1);

    on the RM , Fig 286 , There Are some useful timings on ADC Sampling But clearly , you stop too quickly the conversion. Let me know if you solve your issue. Best Regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    nooshin_1382
    Associate III
    Jun 2, 2015 6:05 AM UTC
    Posted on June 02, 2015 at 08:05

    Hi Erwan

    I tested the ADC in SPC560B54L5 and it is worked thanks so much.

    But i read the Document you refer me I set ADC timming correctlly like a datasheet but has no effect in SPC560B50L5

    the SpcStudio has no any sample for this chip and this chip completly diffrent with other MCU family.

    thanks so much

    With Best Regards

    Nazerian Vanima
    Erwan YVIN
    ST Technical Moderator
    Jun 2, 2015 1:13 PM UTC
    Posted on June 02, 2015 at 15:13

    Hello Vanima ,

    the difference is linked to the flash not the ADC ip.

    Did you use a MiniModule or Discovery Board ?

    You can find in the attachment , your application updated.

    did you try an other HW ?

              Best Regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.