Skip to main content
nooshin_1382
Associate III
Sep 8, 2015 7:40 AM UTC
Question

Bug on SPC Studio Compiler (Critical Error )

Posted on September 08, 2015 at 09:40

Hi

I write a bootloader program for my device the program compiled ok when i choose this option ( LOAD IN RAM ) the program complied ok and run successful

but when i choose the seconde option(Copy in RAM ) the compiler build a bin file with 1GB size

and when i choose the first option (Execute From Flash ) if i select the 0x0000 address the program compile ok but when i select the other section like 128K code section the program not compile and get me this error

input section'.sdata' = 'awsl'

output section '.data' ='awl'

c:/spc5studio/eclipse/plugins/com.st.tools.spc5.tools.hightec.win32_1.0.0.201306281422/hightec/bin/../lib/gcc/ppc-ht-eabi/4.6.3/../../../../ppc-ht-eabi/bin/ld.exe: build/out.elf section `.boot0' will not fit in region `flash'

c:/spc5studio/eclipse/plugins/com.st.tools.spc5.tools.hightec.win32_1.0.0.201306281422/hightec/bin/../lib/gcc/ppc-ht-eabi/4.6.3/../../../../ppc-ht-eabi/bin/ld.exe: region `flash' overflowed by 5787888 bytes

collect2: ld returned 1 exit status

make: *** [build/out.elf] Error 1

I use SPC560B50L5

Thanks For help

Best Regards

Nazerian Vanima
    This topic has been closed for replies.