Skip to main content
nooshin_1382
Associate III
Mar 16, 2015 6:15 PM UTC
Question

Bug in SPCstudio Complier or SPC MCU Family

Posted on March 16, 2015 at 19:15

Hi

I want to use 2 can port , i tried a lot for this issue in two MCU :

SPC560B50L5 and SPC560B54L5 Both of them Have a same Response

in this family when i look at the datasheet i saw a Flexcan1 have 3 CANRX pin And 2 CANTX pin  in program you can set the function of pin for can driver when you set pins manualy or set with pinmap .

Finally I found the Special pins for can is work correctly :

only PC[10] =CANTX1 and PC[3] =CANRX1 

the Refrence manual and datasheet said you can select the pin  but it is not correct

is this bug or not ?

best regards

Vanima
    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Mar 18, 2015 8:48 AM UTC
    Posted on March 18, 2015 at 09:48

    Hello Vanima ,

    In fact , the Reference Manual is not cleared .

    You have to configure the PADSEL (Cf Table 149)

    [DEAD LINK /public/STe2ecommunities/mcu/Lists/SPC56/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/SPC56/Problem%20with%20Flexcan2%20and%20Flexcan3%20in%20spc560b50L5&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000C7B65FFB6DB42540A4DAECE852348058&TopicsView=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/SPC56/AllItems.aspx&currentviews=14]https://my.st.com/public/STe2ecommunities/mcu/Lists/SPC56/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSPC56%2fProblem%20with%20Flexcan2%20and%20Flexcan3%20in%20spc560b50L5&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000C7B65FFB6DB42540A4DAECE852348058&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSPC56%2FAllItems%2Easpx&currentviews=14

       Best Regards

                      Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    nooshin_1382
    Associate III
    Mar 19, 2015 10:43 AM UTC
    Posted on March 19, 2015 at 11:43

    Hello Erwan

    Thanks a lot , it is completely  solved my problem and very usefull .

    with Best Regards

    Vanima