Associate III
Jul 10, 2019 6:33 AM UTC
Question
bootloader jump to application not working
- 1 reply
- 1053 views
Hi,
Kindly Refer the attachments.
Can you figure am I doing something wrong on jump to application program? (refer main.c)
Here, the code is flashed in address 0x00008000 as expected, but jump to application is not done. The flash area of the actual PIT program as well, starts from 0x00008000, so I presume, there shouldn't be a problem. (refer flash.png
But the program counter points to 0x400003B0, which is a RAM area. (refer PC.png)
Could you please help me in,
- Performing Jump to Application program
- Relocating vector table to point the interrupts to the application program
Best Regards,
Prashanth Mohan