Skip to main content
Associate III
Feb 12, 2024 11:30 AM UTC
Solved

board.c generation

Hi

I have an imported project and I would like to modificy the GPIO configuration inside board.c

I saw board.c is a file generated from pinMapEditor configuration but is I open the project and the PinMapEditor page I'm not able to modify anything because the pin configuration setting does not open and clicking on the pin name does nothing happen.

Any suggestion?

Thanks

Fabio

 

 

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Feb 12, 2024 1:46 PM UTC

Hi,

If you imported the project from existing samples, you cannot modify it.

You need to create a new project adding the same components and configuration. 

Then in the PinMap editor you will be able to right-click and change the pin assignment.

Make sure to keep the same pin name otherwise you need to change the pin name in the source code too.

Best Regards,

AutoDevKit Team

2 replies

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Feb 12, 2024 1:46 PM UTC

Hi,

If you imported the project from existing samples, you cannot modify it.

You need to create a new project adding the same components and configuration. 

Then in the PinMap editor you will be able to right-click and change the pin assignment.

Make sure to keep the same pin name otherwise you need to change the pin name in the source code too.

Best Regards,

AutoDevKit Team

Associate III
Feb 14, 2024 3:37 PM UTC

Thanks Max,

 

I directly changed the configuration.xml

 

Fabio