Skip to main content
Mahesh Chamaraja
Associate II
Jan 25, 2017 1:58 PM UTC
Question

Based on FlexRay communication driver development for SPC564A80B4

Posted on January 25, 2017 at 14:58

Hello all,

We are facing some difficulties with FlexRay driver development for SPC564A80B4.

  • We can able to configure the Protocol Control Registers (PCR0~31) for FR configurations, so that ECU and FlexRay module successfully able to move to Normal Active state of Flexray communication.

  • Also message buffer configurations for Transmission and reception is also performed according to number slots.

  • Tool (CANalyser) is also configured with the same flexray configurations as ECU.

  • Now, when we are sending a frame from ECU in slot 64 (dynamic slot).

  • But we observed frame error/ SERR error in the CANlyser window, also payload length is observed as zero and slot ID is 64 is visible. (Please find the attached error snapshot SERR_error.jpg)

     

We would like to know what can be the possible reasons for this error.

Please let us know if any additional information is required.

Regards 

Mahesh C

#flexraycommunication-driver-development-for-spc564a80b4
    This topic has been closed for replies.

    6 replies

    Erwan YVIN
    ST Technical Moderator
    Jan 26, 2017 3:05 PM UTC
    Posted on January 26, 2017 at 16:05

    Hello Manesh ,

    According to the RM, in the chapter 33.4.2

    If the protocol engine is clocked by the internal PLL, the frequency of the PE clock source is

    system clock / 3. The system clock frequency has to be 120 MHz.

    Did you clock your protocol Engine Clock ? on-chip crytal simulator or PLL ?

    CLKSEL

    Protocol Engine Clock Source Select �? This bit is used to select the clock source for the protocol

    engine.

    0 PE clock source is generated by on-chip crystal oscillator

    1 PE clock source is generated by on-chip PLL

    Have you checked the different Status Register , Message Buffer Status Error and Channel A/B Status error?

        Best Regards

                           Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Mahesh Chamaraja
    Associate II
    Jan 27, 2017 10:49 AM UTC
    Posted on January 27, 2017 at 10:49

    Hello Erwan,

    We using ext-crystal osc of 40Mhz as a PE clock.

       0690X000006069wQAA.png0690X00000606A1QAI.png

    Erwan YVIN
    ST Technical Moderator
    Feb 1, 2017 3:23 PM UTC
    Posted on February 01, 2017 at 15:23

    Hello Mahesh ,

    it is often a question of configuration , timing settings.

    FlexRay is a difficult IP, with just bad timing setting , nothing can work.

    I am checking with experts.

       Best regards

                Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Erwan YVIN
    ST Technical Moderator
    Feb 2, 2017 9:01 AM UTC
    Posted on February 02, 2017 at 10:01

    Hello Mahesh ,

    Honestly , you should try to solve your clock configuration (loss of clock) first because a timing issue on Flexray ip could trigger some synchro issues.

    https://community.st.com/0D50X00009XkYOySAN

    Did you use official AutoSAR Flexray MCAL driver ?

    or it is your own driver ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Mahesh Chamaraja
    Associate II
    Feb 2, 2017 1:48 PM UTC
    Posted on February 02, 2017 at 13:48

    Hello Erwan,

    Our own driver

    Regards

    Mahesh