Skip to main content
szhan.7
Associate II
Sep 27, 2022 3:14 AM UTC
Solved

Application configuration

when i configure spc58nn project ,there is pineditor and clock tree ,the configurtion gui. and i cant find any other peripheral configuration gui,any one know this?

    This topic has been closed for replies.
    ODOUV.1
    ODOUV.1Best answer
    ST Employee
    Sep 27, 2022 8:00 AM UTC

    select platform:0693W00000SwKFYQA3.pngthen click on +:0693W00000SwKFxQAN.pngthen select GTM:0693W00000SwKG7QAN.png

    11 replies

    ODOUV.1
    ST Employee
    Sep 27, 2022 6:17 AM UTC

    Hello,

    did you import an existing SPC58xNxx project ?

    or did you created a new SPC58xNxx project ?

    What would you need that you do not see ?

    Best Regards.

    ODOUV.1
    ST Employee
    Sep 27, 2022 6:31 AM UTC

    Select the Platform component and click on the Green "+" to add others components (Init and LowLevelDrivers)

    szhan.7
    szhan.7Author
    Associate II
    Sep 27, 2022 7:29 AM UTC

    0693W00000SwJlOQAV.png0693W00000SwJlnQAF.pngi import example project,there are only two items above,and i want to know if there is any other peripheral wizard,such as canfd ,SDADC or GTM and so on.

    szhan.7
    szhan.7Author
    Associate II
    Sep 27, 2022 6:35 AM UTC

    0693W00000SwJlOQAV.png0693W00000SwJlnQAF.pngi import example project,there are only two items above,and i want to know if there is any other peripheral wizard,such as canfd ,SDADC or GTM and so on.

    ODOUV.1
    ST Employee
    Sep 27, 2022 7:29 AM UTC

    There are no other Graphical tools.

    To configure SDADC or CAN, you need to add and configure the Low Level Drivers component:0693W00000SwK41QAF.pngFor GTM, you need to add and configure the GTM component:0693W00000SwK4LQAV.png 

    You can take a look at GTM examples:0693W00000SwK4uQAF.png

    szhan.7
    szhan.7Author
    Associate II
    Sep 27, 2022 7:52 AM UTC

    I can see low level Drivers component RLA,but i cant find GTM compennent==

    ODOUV.1
    ODOUV.1Best answer
    ST Employee
    Sep 27, 2022 8:00 AM UTC

    select platform:0693W00000SwKFYQA3.pngthen click on +:0693W00000SwKFxQAN.pngthen select GTM:0693W00000SwKG7QAN.png

    szhan.7
    szhan.7Author
    Associate II
    Sep 27, 2022 8:12 AM UTC

    thank you very much :grinning_face:

    ODOUV.1
    ST Employee
    Sep 27, 2022 9:01 AM UTC

    you are welcome ;)

    ODOUV.1
    ST Employee
    Sep 27, 2022 9:12 AM UTC

    click onimport samples0693W00000SwKmNQAV.png0693W00000SwKmXQAV.png0693W00000SwKmcQAF.pngbutton NEXT

    0693W00000SwKmwQAF.png0693W00000SwKn6QAF.pngbutton FINISH