Skip to main content
ivancolla9
Associate III
Feb 29, 2016 3:12 PM UTC
Question

ADC convertion when input 0 voltage

Posted on February 29, 2016 at 16:12

Good morning to everyone,

I am trying to understand a possible problem I have with tha AD converter of the SPC56ELxx.

I am working on a board where an input current is used to set an input voltage to trhe ADC converter of the micro controller. 

The ADC seems to work fine: I tested the vlaues in the channel data and they seem right.

But if the input voltage is 0, the AD converter give me a valid DATA, 0x2BB. 

The circuit should  give a voltage proportional to the input current, so, if the current is 0, I expect to read 0 on the ADC channel data.

Is there some characteristic of the ADC converter that I don't know, so that, if the input voltage is 0, it write in the data channel a different value (something like a low treshold)?

Thanks,

Ivan

#ad-converter #low-treshold
This topic has been closed for replies.

2 replies

Erwan YVIN
ST Technical Moderator
Apr 8, 2016 11:57 AM UTC
Posted on April 08, 2016 at 13:57

Hello Ivan ,

did you solve the issue ?

i have no problem onSPC56ELxx OS-Less ADC Test Application for DiscoveryPlus

the ADC Conversion is well 0x0 or 0x1.

(cf screenshot)

for standard channel, i recommend you to increase INPSAMP.

Best regards

Erwan

________________

Attachments :

2016-04-08_135453.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtZg&d=%2Fa%2F0X0000000aRv%2FTJPG9LN0xDNrV0gsb1Z0YrX_exlnoC9g1S0sJAKZ3H8&asPdf=false
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ivancolla9
Associate III
May 3, 2016 3:42 PM UTC
Posted on May 03, 2016 at 17:42

Hello Erwan,

I worked on the problem and discovered that it was caused by the external circuitry on wich the controller is embedded. I learned how to manage the ADC and now I have no problems.

Regards,

Ivan