Skip to main content
fastfret
Visitor II
Nov 2, 2020 9:12 AM UTC
Solved

About SPC58 flash programming?

I would like to implement the flash programming to our JTAG tool.

Are there any documents that describe OnCE module and the Nexus read/write (R/W) access block?

Such as those described in AN4035. The only thing that AN4035 is inapplicable for SPC58 device.

Thanks all.

​

​

    This topic has been closed for replies.
    Giuseppe DI-GIORE
    ST Employee
    Nov 2, 2020 12:13 PM UTC

    Hello,

    actually a flash programmer is implemented downloading a piece of code in RAM communicating with the host PC via JTAG and able to program the flash.

    The code n RAM includes a device specific flash driver.

    So, have a look at one of the Reference Manuals of the SPC58 devices, the section JTAG Controller.

    Just for example, reference manual of SPC582B is available here:

    https://www.st.com/content/ccc/resource/technical/document/reference_manual/group0/04/88/e1/3e/9a/3b/4f/54/DM00201129/files/DM00201129.pdf/jcr:content/translations/en.DM00201129.pdf

    Regards,

    Giuseppe

    1 reply

    Giuseppe DI-GIORE
    ST Employee
    Nov 2, 2020 12:13 PM UTC

    Hello,

    actually a flash programmer is implemented downloading a piece of code in RAM communicating with the host PC via JTAG and able to program the flash.

    The code n RAM includes a device specific flash driver.

    So, have a look at one of the Reference Manuals of the SPC58 devices, the section JTAG Controller.

    Just for example, reference manual of SPC582B is available here:

    https://www.st.com/content/ccc/resource/technical/document/reference_manual/group0/04/88/e1/3e/9a/3b/4f/54/DM00201129/files/DM00201129.pdf/jcr:content/translations/en.DM00201129.pdf

    Regards,

    Giuseppe