Skip to main content
guo qiang
Senior
Sep 25, 2017 12:53 PM UTC
Question

A question about irqIsrEnable Function

Posted on September 25, 2017 at 14:53

I wrote a BootLoader program. and a APP 

program

I downloaded the BootLoader to the 0x0 address in Flash By UDE 4.8.

I downloaded the App to the 0x18000 address in Flash By UDE 4.8.

//code 1:

componentsInit();

irqIsrEnable();

SPCSetRunMode(SPC5_RUNMODE_DRUN);

 irqIsrDisable();

asm volatile (''e_lis %r3, 0x00018008@h \t\n''

''e_or2i %r3, 0x00018008@l \t\n''

''mtctr %r3 \t\n''

''se_bctrl'');

//APP:

componentsInit();

irqIsrEnable();

for ( ; ; )

{

  pal_lld_togglepad(PORT_C, PC_LED8);

  osalThreadDelayMilliseconds(1000);

}

Everything is OK.

But ,If i am use CAN in the Bootload .when the APP run to irqIsrEnable

.it will be enter 

_unhandled_irq function

//code 2:

componentsInit();

irqIsrEnable();

can_lld_start(&CAND1,&can_config_cfg0);

SPCSetRunMode(SPC5_RUNMODE_DRUN);

 irqIsrDisable();

asm volatile (''e_lis %r3, 0x00018008@h \t\n''

''e_or2i %r3, 0x00018008@l \t\n''

''mtctr %r3 \t\n''

''se_bctrl'');

//APP:

componentsInit();

irqIsrEnable();

for ( ; ; )

{

  pal_lld_togglepad(PORT_C, PC_LED8);

  osalThreadDelayMilliseconds(1000);

}0690X00000608MiQAI.png0690X00000608N2QAI.png

I think that before the jump to close the CAN, APP implementation irqIsrEnable will continue to run.but  i try call can_lld_stop.andt jump to APP ,it doesn't work..

pls help me !

    This topic has been closed for replies.

    3 replies

    Erwan YVIN
    ST Technical Moderator
    Sep 26, 2017 8:35 AM UTC
    Posted on September 26, 2017 at 10:35

    Hello ,

    You have to switch in assembler mode in debug PLS tool

    and check to the register LR (Link register) to check the cause of the issue.

                  Best regards

                                   Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    guo qiang
    guo qiangAuthor
    Senior
    Sep 26, 2017 12:55 PM UTC
    Posted on September 26, 2017 at 12:55

    open fae_debg.wsx file using PLS 4.8

    ________________

    Attachments :

    SPC560B_BootLoad_APP_Test.7z.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyP7&d=%2Fa%2F0X0000000b7G%2FNIHGuTrnaQmC4F7_ZxFo8hOY898EpGBrtDa4Z_NJxBI&asPdf=false
    procolo
    Visitor II
    Sep 26, 2017 2:08 PM UTC
    Posted on September 26, 2017 at 16:08

    Hi

    please do not call can_stop . there is an issue we are tring to understand

    check here:

    https://community.st.com/0D50X00009XkXx9SAF