Skip to main content
PLEE.2
Associate II
Feb 6, 2023 4:56 PM UTC
Question

1byte write in flash

i use SPC58EC80E1

if feature : flash size 4MB

​the flash Consisted of low block, lager block, high block.

I want to write 4byte for low block (0xfc0000) in test1_func().

continuously, I want to write 4byte for low block (0xfc0004) in test2_func()

For example)

flash_low_block_erase(2); //0xfcc0000 erase

one_word_write(0xffc0000,0x12345678);

one_word_write(0xffc0004,0x9abcdef0);

​

onr_word_write(uint32 address, uint32 value)

{

tt_buffer[0] = value;

/* /* for write is byte unit, UINT32 tt_buffer : 0x04 */

returnCode = FlashProgram(&ssdConfig, FALSE, targetAddress, 4, &tt_buffer[0],

&pgmCtxData);

​

if (C55_OK == returnCode) {

// // Call FlashCheckStatus() to check status of the progress

while (C55_INPROGRESS == FlashCheckStatus(&ssdConfig,

C55_MODE_OP_PROGRAM, &opResult, &pgmCtxData)) {

//Add your code here

}

​

if (C55_OK != opResult) {

ErrorTrap(opResult);

}

} } else {

ErrorTrap(returnCode);

}

​

returnCode = ProgramVerify(&ssdConfig, targetAddress, 4, &tt_buffer[0], &failAddress,&failData, &failSource, &pvCtxData);

​

if (C55_OK == returnCode) {

/ /Call FlashCheckStatus() to check status of the progress

while (C55_INPROGRESS == FlashCheckStatus(&ssdConfig,

C55_MODE_OP_PROGRAM_VERIFY, &opResult, &pvCtxData)) {

//Add your code here

}

​

if (C55_OK != opResult) {

ErrorTrap(opResult);

}

}

} else {

ErrorTrap(returnCode);

}

}

But, do memory dump

SD:00FCC0000 : 12345678 FFFFFFFF FFFFFFFF .....

​

Of course, if you use 0x12345678 0x9abcdef0 continuously, it works well.

tt_buffer[0] =0x12345678;

tt_buffer[1] = 0x9abcdef0;

ProgramVerify(&ssdConfig, 0xFC0000, 8, &tt_buffer[0], ....

==> dump : SD:00FCC0000 : 123456789abcdef0 FFFFFFFF .....

So, I want to know if I write to a specific address in flash at least once, I can't use it again in the area around it.

If not, I want to know if there is a solution.

​

thanks

best regards.

PLEE​

This topic has been closed for replies.

1 reply

PLEE.2
PLEE.2Author
Associate II
Feb 7, 2023 4:05 AM UTC

problem solved