Skip to main content
WMa.2
Associate II
Dec 8, 2022 8:30 AM UTC
Solved

Where is the path of the spc5studio header file

0693W00000WKWlRQAX.pngWhy can't I include the system standard header files? Why can I generate files even if there are problems as long as the console is fine when compiling? Finally, I can burn the program into the chip and run it successfully.0693W00000WKWlHQAX.png0693W00000WKWl2QAH.png0693W00000WKWkxQAH.png0693W00000WKWgbQAH.png0693W00000WKWgWQAX.png

    This topic has been closed for replies.
    Max VIZZINI
    Max VIZZINIBest answer
    ST Technical Moderator
    Dec 12, 2022 9:06 AM UTC

    Dear Sir,

    These standard types include are not needed because they are managed internally by SPC5Studio to deal with different compilers and to comply to MISRA rules.

    In addition, anything is under the source folder in the project is compiled.

    Finally, you can change compiling and linking options from the configuration of the platform.

    Best Regards,

    AutoDevKit Team

    1 reply

    Max VIZZINI
    Max VIZZINIBest answer
    ST Technical Moderator
    Dec 12, 2022 9:06 AM UTC

    Dear Sir,

    These standard types include are not needed because they are managed internally by SPC5Studio to deal with different compilers and to comply to MISRA rules.

    In addition, anything is under the source folder in the project is compiled.

    Finally, you can change compiling and linking options from the configuration of the platform.

    Best Regards,

    AutoDevKit Team