Skip to main content
Associate III
May 20, 2024 6:46 AM UTC
Solved

want to know the CAN BUSOFF is implemented or not In "Avas Compact - Test Application".

hi community,

                      I am using the "Avas Compact - Test Application" example code which is provided in the AUTODEVKIT. hear I enabled the CAN communication and it is working fine. but i want to know CAN BUSOFF is implemented or not in the given example code. if not how to implement the CAN BUSOFF.

regards

shiva

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
May 20, 2024 8:57 AM UTC

Hi,

>>    i just want to know the "CAN BUSOFF" is implemented or not.

No, not implemented.

Best Regards,

AutoDevKit Team

3 replies

Max VIZZINI
ST Technical Moderator
May 20, 2024 6:56 AM UTC

hi,

In the original code, the CAN messages are used to increase/decrease volume and engine speed and not to start/stop the sound.

There is a button on the board to start the engine. You should implement a similar code to start the engine with a CAN message.

Best Regards,

AutoDevKit Team

Associate III
May 20, 2024 8:48 AM UTC

hi 

    i just want to know the "CAN BUSOFF" is implemented or not.

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
May 20, 2024 8:57 AM UTC

Hi,

>>    i just want to know the "CAN BUSOFF" is implemented or not.

No, not implemented.

Best Regards,

AutoDevKit Team