Skip to main content
Associate III
May 20, 2024 6:34 AM UTC
Solved

Timeout functions

Hi community,

I have implemented AVAS, I am getting the output as expected but with one issue that even after I stop communication in the CANoe , I am getting the sound continuously.

I wanted to know two things

1. Do we have any API that stops the sound just after stopping the communication in CANoe?

2. I thought of using the timeout functions that gets called after some time after stopping the communication so for this I wanted to know do we have any API or do we have any configuration settings?

 

Thanks,

Aishwarya UM

 

 

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
May 20, 2024 8:54 AM UTC

Hi,

>>1. I wanted to know do we have any API that particularly meant for activating and deactivating the Sound as like the >>hardware button(I mean I want a API which works as hardware button).

No, there is no API.

>>2. If there is no any such API,s then I am planning to use timeout function so I wanted to know is there any timeout >>API's or do I need to modify the configurations so that timeout API's gets enabled if any.

No, there is not such an API.

Best Regards,

AutoDevKit Team

 

 

 

3 replies

Max VIZZINI
ST Technical Moderator
May 20, 2024 6:58 AM UTC

Hi,

No there is no CAN message to start/stop the sound.

See answer to similar question in the above post.

Best Regards,

AutoDevKit Team

Associate III
May 20, 2024 8:17 AM UTC

Hi Max Vizzini,

I think you took the question in the other way. I am not asking about the CAN message that we need for start/stop sound. actually I have used entirely different messages and signals for my coded. I am not using the existing messages that are available in the base source code.

My doubt is,

1. I wanted to know do we have any API that particularly meant for activating and deactivating the Sound as like the hardware button(I mean I want a API which works as hardware button).

2. If there is no any such API,s then I am planning to use timeout function so I wanted to know is there any timeout API's or do I need to modify the configurations so that timeout API's gets enabled if any.

 

Thanks,

Aishwarya UM

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
May 20, 2024 8:54 AM UTC

Hi,

>>1. I wanted to know do we have any API that particularly meant for activating and deactivating the Sound as like the >>hardware button(I mean I want a API which works as hardware button).

No, there is no API.

>>2. If there is no any such API,s then I am planning to use timeout function so I wanted to know is there any timeout >>API's or do I need to modify the configurations so that timeout API's gets enabled if any.

No, there is not such an API.

Best Regards,

AutoDevKit Team