Skip to main content
Associate II
Sep 5, 2024 9:20 AM UTC
Solved

SPC582B flashing error

hello team,

I'm using AutodevKit studio for testing AEK_AUD_C1D9031 board.

I imported example code from sample : SPC582Bxx_RLA_AEK_AUD_C1D9031 - Avas Compact - Test Application.

 


but upon flashing board I'm getting this error.

MohitManvar_0-1725527788326.png


kindly provide feedback. for your reference I'm attaching log file.

Mohit M

This topic has been closed for replies.
ATROI
ATROIBest answer
ST Employee
Sep 6, 2024 1:25 PM UTC

Hi MohitManvar,

When you wrote "I am able to flash from other workspace",
does it mean that you're able to flash another project in the same AEK board or different AEK board?
Other things, can you post us the screen shots of the tabs:
Main and SVD Path tabs of the Debug configuration?

 

Thanks,

AutoDevKit Team

5 replies

ATROI
ST Employee
Sep 6, 2024 6:54 AM UTC

 

Hi MohitManvar,

Please could you try to clean and rebuild the project and then try to flash it again.

Thanks, 

AutoDevKit Team

Associate II
Sep 6, 2024 7:03 AM UTC

Hello,

i tried with that but not working. even I tried to re import sample project but that is also not working

Max VIZZINI
ST Technical Moderator
Sep 6, 2024 7:08 AM UTC

Hi,

Please make sure that the board is properly connected with cable working and that it is recognized by UDE (if you are using PLS...).

Best Regards,

AutoDevKit Team

ATROI
ATROIBest answer
ST Employee
Sep 6, 2024 1:25 PM UTC

Hi MohitManvar,

When you wrote "I am able to flash from other workspace",
does it mean that you're able to flash another project in the same AEK board or different AEK board?
Other things, can you post us the screen shots of the tabs:
Main and SVD Path tabs of the Debug configuration?

 

Thanks,

AutoDevKit Team