Skip to main content
Associate
Jul 16, 2024 2:10 AM UTC
Solved

How to erase/write spcific NVM(MCU flash) part with Stellalink+AutoDevKit Studio on AVAS EVK?

Hello,

 

As far as I known, ST released two kinds of AVAS EVK which one is based on AEK-MCU-C1MLIT1(https://www.st.com/en/solutions-reference-designs/sl-ssasf011101v1.html ) and another is based on AEK-AUD-C1D9031(https://www.st.com/en/evaluation-tools/aekd-stereoavas.html#overview ).

I have both EVKs now but I have a issue on #2 case below.

  1. AEK-MCU-C1MLIT1 with PLS Programmer/debugger tool + UDE StarterKit SW
    • As you know well, AEK-MCU-C1MLIT1 board includes PLS Programmer/debugger tool inside itself. So, Under this environment(PLS Programmer/debugger tool + UDE StarterKit SW), I can write/erase specific NVM part to change WAV file(.hex format) and the way is explained very well on UM2719 like below.
       
      decemberdream_0-1721094787947.png

       

      decemberdream_1-1721094787949.png

       

       

  2. AEK-AUD-C1D9031 with StellaLink Programming/Debugging tool + autodevkitspc5studio
    • SWAEK-AUD-C1D9031 board doesn't include PLS Programmer/debugger tool inside itself. So, I bought a stellalink(AEK-AUD-D1D9031 can support this). But Under this environment(StellaLink Programmer/debugger tool + autodevkitspc5studio SW), I don't know how to write/erase specific NVM part to change WAV file(.hex format). I made the environment which can debug with OpenOCD but I can't find any document for NVM erasing/writing...

 

Could you help me from this trouble?

 

Thanks,

This topic has been closed for replies.
ATROI
ATROIBest answer
ST Employee
Jul 16, 2024 8:40 AM UTC
Hi Decemberman,
 
There isn't a script to erase a specific block memory yet, but you could use this one as an example:
 
spc582b_dis_FLASH_ERASE_ALL.cfg.
 
you can find this file under C:\AutoDevKitStudio-2.4.0\openocd\scripts\utility.
 
Read the readme.txt file first. 
 
Replace the command path from: 
 
C:\StellarLINK\openocd\bin\openocd.exe -d0 -s C:\StellarLINK\openocd\scripts -f utility\spc582b_dis_FLASH_ERASE_ALL.cfg
 
to:
 
C:\AutoDevKitStudio-2.4.0\openocd\bin\openocd.exe -d0 -s C:\AutoDevKitStudio-2.4.0\openocd\openocd\scripts -f utility\spc582b_dis_FLASH_ERASE_ALL.cfg.
 
For more info, see the UM of OpenOCD online.
 
Thanks,
AutoDevKit Team

1 reply

ATROI
ATROIBest answer
ST Employee
Jul 16, 2024 8:40 AM UTC
Hi Decemberman,
 
There isn't a script to erase a specific block memory yet, but you could use this one as an example:
 
spc582b_dis_FLASH_ERASE_ALL.cfg.
 
you can find this file under C:\AutoDevKitStudio-2.4.0\openocd\scripts\utility.
 
Read the readme.txt file first. 
 
Replace the command path from: 
 
C:\StellarLINK\openocd\bin\openocd.exe -d0 -s C:\StellarLINK\openocd\scripts -f utility\spc582b_dis_FLASH_ERASE_ALL.cfg
 
to:
 
C:\AutoDevKitStudio-2.4.0\openocd\bin\openocd.exe -d0 -s C:\AutoDevKitStudio-2.4.0\openocd\openocd\scripts -f utility\spc582b_dis_FLASH_ERASE_ALL.cfg.
 
For more info, see the UM of OpenOCD online.
 
Thanks,
AutoDevKit Team