Skip to main content
Associate
Apr 30, 2026 1:51 AM UTC
Solved

How can I connect Lauterbach debugger to AEK-COM-10BASET?

Hello support team,

 

I just received a new AEK-COM-10BASET board and trying to connect Lauterbach debugger with License module for MPC55xx.

 

Question : How can I connect to the board through Lauterbach debugger & SW?

 

Currently the SW (TRACE32) shows error message when I press "Up" button.

apap_2-1777512866787.png

 

I have no idea why such "Target Power Fail" error or "Power Down" message is appeared.

Also I checked below 11 pin and the measured voltage is 3.3V.

apap_3-1777512975847.png

 

The jumper (switch) configuration I made are ;

JP1~JP7 : closed = short

J13, J14 : I tried both 1-2 and 2-3 connection

apap_4-1777513103738.png

 

Any comment is appreciated, thanks!

 

Best regards,

apap

 

 

This topic has been closed for replies.
apapBest answer
Associate
May 7, 2026 1:12 AM UTC

Hello Team,

 

I found wrong cable connection and I successfully connected / started debugging through Lauterbach debugger.

Based on it's default basic CMM script I also flashed the sample project's ELF. Looks like working.

 

Thank you for help!

 

 

 

2 replies

Max VIZZINI
ST Technical Moderator
Apr 30, 2026 9:34 AM UTC

Hi,

We have not tested the board with Lauterbach. We used OpenOCD as deployed in AutoDevKit Studio.

By the way, our MCU is SPC58EC e not MPC55xx. Might this be the difference?

Best Regards,

AutoDevKit Team

apapAuthorBest answer
Associate
May 7, 2026 1:12 AM UTC

Hello Team,

 

I found wrong cable connection and I successfully connected / started debugging through Lauterbach debugger.

Based on it's default basic CMM script I also flashed the sample project's ELF. Looks like working.

 

Thank you for help!