Skip to main content
Bwang.3
Associate III
May 27, 2024 3:17 PM UTC
Solved

Hello! Ask a question about the debugger!

May I use the onboard debugger on the SPC582B-DIS Discovery board to download debugging programs for the AEK-MOT-MR200G1 development board? Can you tell me which specific pins need to be connected? As shown in the following picture!

QQ图片20240527225204.pngQQ图片20240527225444.png

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Jun 4, 2024 3:19 PM UTC

Hi Bwang, 

The following changes are required for programming and debugging the AEK-MOT-MR200G1 board with OpenOCD:

step 1: Under C:\AutoDevKitStudio-2.2.1\openocd\scripts\board open the file spc582b_dis.cfg

step2: at line 12 insert: reset_config srst_push_pull as showed in the image below.

MaxVIZZINI_0-1717514331994.png

 

step3: save the file.

step4: program and debug your code using OpenOCD in AutoDevKIt Studio

 

Thanks,

AutoDevKit Team

2 replies

Max VIZZINI
ST Technical Moderator
May 27, 2024 7:34 PM UTC

Hi,

This kind of connection is too error prone. We do not suggest it.

Best Regards,

AutoDevKit Team

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Jun 4, 2024 3:19 PM UTC

Hi Bwang, 

The following changes are required for programming and debugging the AEK-MOT-MR200G1 board with OpenOCD:

step 1: Under C:\AutoDevKitStudio-2.2.1\openocd\scripts\board open the file spc582b_dis.cfg

step2: at line 12 insert: reset_config srst_push_pull as showed in the image below.

MaxVIZZINI_0-1717514331994.png

 

step3: save the file.

step4: program and debug your code using OpenOCD in AutoDevKIt Studio

 

Thanks,

AutoDevKit Team