Skip to main content
Associate II
Apr 29, 2025 4:46 AM UTC
Solved

error when trying connection to target(SPC58NH-DISP) using AEK-MCU-SPC5LNKU(debugger) and UDE Starterkit 5.02.04

Hello.

 

I'm using SPC58NH-DISP, and trying to debug using AEK-MCU-SPC5LNKU(debugger) and UDE Starterkit 5.02.04.

When I power on SPC58NH-DISP and check if USB driver is installed properly, I can find SPC58NH-DISP works fine and "PLS USB Serial Port" in Windows Device Manager. However, the following error message occurs.

<error message>

Message from component 'UDEDebugServer' :
Unable to establish connection . To correct the situation, check configuration file entries and try again.

Message from component 'PpcJtagTargIntf' :
Can't connect target !

Message from component 'PpcJtagTargIntf' :
No JTAG client found !
Please check:
- target power supply
- JTAG cable connection
- target configuration

 

It seems like the error occurs due to wrong target configuration.

I'm curious about where the menu for target configuration is in UDE Starterkit and how to modify the target configuration for SPC58NH-DISP.

 

Thank you.

This topic has been closed for replies.
allhaveBest answer
Associate II
May 7, 2025 1:46 AM UTC

I was able to solve this problem by uninstalling USB driver and re-installing USB driver, so now, I can program and debug SPC58NH-DISP using AEK-MCU-SPC5LNKU(debugger) and UDE Starterkit 5.02.04.

Thank you.

1 reply

allhaveAuthorBest answer
Associate II
May 7, 2025 1:46 AM UTC

I was able to solve this problem by uninstalling USB driver and re-installing USB driver, so now, I can program and debug SPC58NH-DISP using AEK-MCU-SPC5LNKU(debugger) and UDE Starterkit 5.02.04.

Thank you.