Skip to main content
Associate
Jan 11, 2025 10:32 AM UTC
Solved

Debugging SPC56 with AEK-MCU-SPC5LNKU

I recently bought the STEVAL-TTM002V1 along with the AEK-MCU-SPC5LNKU debugger since it was mentioned support for SPC56 would be available before 2024. However, I haven't been able to get the AEK-MCU-SPC5LNKU debugger to work with the SPC56.

  1. I'm wondering whether the support for SPC56 debugging with the AEK-MCU-SPC5LNKU been officially released?
  2. If support is available, could someone guide me how to get started with debugging the SPC56 using the AEK-MCU-SPC5LNKU? Or should I use SPC5-UDESTK only for now?
  3. Should I use AEK-MCU-SPC5LNKU or AEK-MCU-SPC5LNK? 

Any help would be greatly appreciated!

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Jun 27, 2025 7:58 AM UTC

Hi,

We do not support OpenOCD for SPC56, please refer to our MCU partners for support questions.

Thank you for your understanding.

Best Regards,

AutoDevKit Team

8 replies

Max VIZZINI
ST Technical Moderator
Apr 3, 2025 5:20 PM UTC

Hi,

SPC56 is still not supported for OpenOCD and at the moment we have no available plan due to internal priority changes.

You can use AEK-MCU-SPC5LNKU with standard PLS UDE Debugger.

Best Regards,

AutoDevKit Team

Associate II
Jun 26, 2025 5:15 AM UTC

Hello!

There is a chance that SPC56 will be soon supported for Open OCD?

Regards,

Agustín

Max VIZZINI
ST Technical Moderator
Jun 26, 2025 7:41 AM UTC

Hi,

I doubt honestly, no business trend for this.

Why do not you move to SPC58 Chorus 1M (SPC582B) ?

Best Regards,

AutoDevKit Team

Associate II
Jun 26, 2025 1:29 PM UTC

Hi, we bought a spc56 for budges and application reasons. The data briefs of the AEK-MCU-SPC5LNK indicated that in 2024 there will be support for the SPC56 series, so I would like to know if there the config files are the only problem, or there is a hardware problem also.

Thanks for your answer,

Agustin