Skip to main content
Associate II
Dec 5, 2025 4:39 PM UTC
Solved

Availability of High-Level BMS APIs (AEK_POW_BMS63EN) in AutoDevKit

Hello,

In the AEK-POW-BMSCHAIN example code, I see high-level APIs like:

 
AEK_POW_BMS63EN_GetModule() AEK_POW_BMS63EN_init()

But in my AutoDevKit installation, only low-level chain APIs (AEK_POW_BMS63CHAIN_*) are available.

Could you clarify:

  1. Are the high-level AEK_POW_BMS63EN APIs included in the public AutoDevKit package?

  2. If not, are they only available via partner/NDA packages?

  3. Should regular users implement high-level functionality using only the low-level APIs?

Thanks!

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Dec 6, 2025 4:15 PM UTC

Hi,

No, there is no reserved code / package.

The code is available for evaluation purposes.

If you need design support to your coding, you can consult with our partner https://www.beond.net/electronics/ 

Best Regards,

AutoDevKit Team

1 reply

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Dec 6, 2025 4:15 PM UTC

Hi,

No, there is no reserved code / package.

The code is available for evaluation purposes.

If you need design support to your coding, you can consult with our partner https://www.beond.net/electronics/ 

Best Regards,

AutoDevKit Team