Skip to main content
Visitor II
May 14, 2025 8:36 PM UTC
Solved

AutoDevKit Integration & Java VM Error – SPC5 Studio / SPC5-MCTK-01

Hi everyone,

I'm working on a university project involving vehicle lateral control using the SPC5-MCTK-01 board. I'm using SPC5 Studio and AutoDevKit, but I'm facing issues with the setup:

  • AutoDevKit installation via SPC5 Studio (Help → Install New Software) fails repeatedly.

  • Launching AutoDevKit directly results in:
    "Error: Could not create the Java Virtual Machine. A fatal exception has occurred. Program will exit."

Tested on both Windows 10 and 11 – same issue.

I'd appreciate help with:

  • Correct integration of AutoDevKit into SPC5 Studio

  • Fixing the Java VM error

  • Tips or resources for using SPC5-MCTK-01 efficiently

Thanks in advance!
Best regards

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
May 16, 2025 7:30 AM UTC

Hi,

Just to clarify, SPC5-MCTK-01 is not in the AutoDevKit ecosystem therefore you should use pure SPC5Studio.

If you would like to evaluate 3Phase motor control solution in AutoDevKit, I suggest to use AEK-MOT-3P99081 

https://www.st.com/en/evaluation-tools/aek-mot-3p99081.html 

or equivalent AEK-MOT-3P9908M.

Best Regards,

AutoDevKit Team

1 reply

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
May 16, 2025 7:30 AM UTC

Hi,

Just to clarify, SPC5-MCTK-01 is not in the AutoDevKit ecosystem therefore you should use pure SPC5Studio.

If you would like to evaluate 3Phase motor control solution in AutoDevKit, I suggest to use AEK-MOT-3P99081 

https://www.st.com/en/evaluation-tools/aek-mot-3p99081.html 

or equivalent AEK-MOT-3P9908M.

Best Regards,

AutoDevKit Team